Other Parts Discussed in Thread: CONTROLSUITE
Hello,
My application includes packed structures to make communication easier. I am using the C2000 launchpad and CCS 5.4.0.00091.
The compiler reference spru514e states that "The following type attributes are supported: aligned, deprecated, packed, transparent_union, and unused." on page 115, but the compiler itself complains:
invalid attribute for "struct <unnamed>"
with the struct defined as follows:
typedef struct
{
uint8_t len;
uint8_t data;
} __attribute__ ((packed)) comm_t;
Currently the compiler is TI v6.1.3. Are packed structures supported? I've seen several past posts that support would be added (two years ago or so).
Thanks.