Hi,
I am a little bit in doubt about the max baud rate for the 2806x SPI and SCI:
When having a system clock of 90MHz and also LSPCLK at 90MHz, I could get
SCI: max.Baudrate=LSPCLK/16 (BRR=0 or 1) = 5.625 MHz
SPI: max.Baudrate=LSPCLK/4 (SPIBRR=0..3) = 22.5 MHz
In the datasheets sprs698d and spruh18d, I found no limits for SCI, so the 5,625 MHz seems to be okay !?
I found limits for the SP:
Master mode transmit 20-MHz MAX, master mode receive 10-MHz MAX
Slave mode transmit 10-MHz MAX, slave mode receive 10-MHz MAX.
The general GPIO limits are given as max. 20MHz toggling frequency.
So what is the SPI limit? Can it be operated with a 90MHz LSPCLK? Does the baudrate have to be at <= 10MHz (SPIBRR=8) ?
I think, the datasheet is not really clear about this.
For McBSP in SPI mode, I found "With maximum LSPCLK speed of 90 MHz, CLKX maximum frequency is LSPCLK/16 , that is 5.625 MHz".
Any help is appreciated.