This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28335 Memory map tool and RAM



I implementing MODBUS at F28335 DSP but I need 256k of space (the addresses from 0x00000 to 0x50000) to full implement it. At memory map tool I see there is a space called RAM which goes from 0x100000 to 0x2FFFFF. The problem is: I can´ modify it. This memory is locked or something like that? And, if it is, I can only use the RAM to implement the MODBUS?