This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use of FatFs with TMS320F28335

Hi, i'm trying to use FatFs library to read/write on uSD.
My actual code is this:

 
 FATFS Fatfs; /* File system object */  
 FIL file1;  
 f_mount(&Fatfs, "0:", 0);  
 f_open(&file1, "test.txt", FA_OPEN_EXISTING | FA_READ);  



 


f_mount return FR_OK but f_open return always FR_NOT_READY.

I use a SD card of 4GB from Kingston which is a microSD in an SD adaptator which is linked to my DSC.

What can I do ? Thanks

  • I think it is my diskio.c which is not really clear for me which is not adapted to the TMS320F28x.

    So is there any place to download this diskio for TMS because it contains the function disk_initialize which is really important...Thank you very much...

  • I give you the diskio.c I have and which doesn't work...because of the FR_NOT_READY response of f_open...--' Thank you very much to help me.

    /*-----------------------------------------------------------------------*/
    /* Low level disk I/O module skeleton for FatFs     (C)ChaN, 2013        */
    /*-----------------------------------------------------------------------*/
    /* If a working storage control module is available, it should be        */
    /* attached to the FatFs via a glue function rather than modifying it.   */
    /* This is an example of glue functions to attach various exsisting      */
    /* storage control module to the FatFs module with a defined API.        */
    /*-----------------------------------------------------------------------*/
    
    
    
    /*
     * This file was modified from a sample available from the FatFs
     * web site. It was modified to work with a Stellaris DK-LM3S9B96 board.
     */
    
    #include "DSP28x_Project.h"
    #include "diskio.h"
    #include "..\lib\Comm_Spi.h"
    #include "stdbool.h"
    
    
    /*-----------------------------------------------------------------------*/
    /* MMC/SDC (in SPI mode) control module  (C)ChaN, 2007                   */
    /*-----------------------------------------------------------------------*/
    /* Only rcvr_spi(), xmit_spi(), disk_timerproc() and some macros         */
    /* are platform dependent.                                               */
    /*-----------------------------------------------------------------------*/
    
    
    
    /*
     * The following header defines the hardware connections used to connect
     * the SDCard.  This can be found under the relevant board directory.
     */
    
    
    /* Definitions for MMC/SDC command */
    #define CMD0    (0x40+0)    	// GO_IDLE_STATE
    #define CMD1    (0x40+1)    	// SEND_OP_COND
    #define CMD8    (0x40+8)    	// SEND_IF_COND
    #define CMD9    (0x40+9)    	// SEND_CSD
    #define CMD10    (0x40+10)    	// SEND_CID
    #define CMD12    (0x40+12)    	// STOP_TRANSMISSION
    #define CMD16    (0x40+16)    	// SET_BLOCKLEN
    #define CMD17    (0x40+17)    	// READ_SINGLE_BLOCK
    #define CMD18    (0x40+18)    	// READ_MULTIPLE_BLOCK
    #define CMD23    (0x40+23)    	// SET_BLOCK_COUNT
    #define CMD24    (0x40+24)    	// WRITE_BLOCK
    #define CMD25    (0x40+25)    	// WRITE_MULTIPLE_BLOCK
    #define CMD41    (0x40+41)    	// SEND_OP_COND (ACMD)
    #define CMD55    (0x40+55)    	// APP_CMD
    #define CMD58    (0x40+58)    	// READ_OCR
    
    
    
    /*#define CMD0      0x4000    // GO_IDLE_STATE
    #define CMD1      0x4100    // SEND_OP_COND
    #define CMD8      0x4800    // SEND_IF_COND
    #define CMD9      0x4900    // SEND_CSD
    #define CMD10     0x4A00    // SEND_CID
    #define CMD12     0x4C00    // STOP_TRANSMISSION
    #define CMD16     0x5000    // SET_BLOCKLEN
    #define CMD17     0x5100    // READ_SINGLE_BLOCK
    #define CMD18     0x5200    // READ_MULTIPLE_BLOCK
    #define CMD23     0x5700    // SET_BLOCK_COUNT
    #define CMD24     0x5800    // WRITE_BLOCK
    #define CMD25     0x5900    // WRITE_MULTIPLE_BLOCK
    #define CMD41     0x6900    // SEND_OP_COND (ACMD)
    #define CMD55     0x7700    // APP_CMD
    #define CMD58     0x7A00    // READ_OCR*/
    
    
    
    
    
    
    // asserts the CS pin to the card
    static
    void SELECT (void)
    {
    
    	//TODO: Pull CS low
    //    //
    //    // Make sure that the serial flash which shares this SSI port is
    //    // not selected.
    //    //
    //    GPIOPinWrite(SFLASH_CS_BASE, SFLASH_CS_PIN, SFLASH_CS_PIN);
    //
    //    //
    //    // Select the SD card.
    //    //
    //    GPIOPinWrite(SDCARD_CS_BASE, SDCARD_CS_PIN, 0);
    
    	GpioDataRegs.GPADAT.bit.GPIO19 = 0;
    }
    
    // de-asserts the CS pin to the card.
    static
    void DESELECT (void)
    {
    	//TODO: Pull CS High
    //    GPIOPinWrite(SDCARD_CS_BASE, SDCARD_CS_PIN, SDCARD_CS_PIN);
    	GpioDataRegs.GPADAT.bit.GPIO19 = 1;
    }
    
    /*--------------------------------------------------------------------------
    
       Module Private Functions
    
    ---------------------------------------------------------------------------*/
    
    static volatile
    DSTATUS Stat = STA_NOINIT;    /* Disk status */
    
    static volatile
    BYTE Timer1, Timer2;    /* 100Hz decrement timer */
    
    static
    BYTE CardType;            /* b0:MMC, b1:SDC, b2:Block addressing */
    
    static
    BYTE PowerFlag = 0;     /* indicates if "power" is on */
    
    /*-----------------------------------------------------------------------*/
    /* Transmit a byte to MMC via SPI  (Platform dependent)                  */
    /*-----------------------------------------------------------------------*/
    
    static
    void xmit_spi (BYTE dat)
    {
    //    DWORD rcvdat;
    //
    //    SPIDataPut(&SpiaRegs, dat); /* Write the data to the tx fifo */
    //
    //    SPIDataGet(&SpiaRegs, (unsigned int *) &rcvdat); /* flush data read during the write */
    
    	/*spi_xmit(&SpiaRegs, dat << 8);*/
    
    	//SpiaRegs.SPITXBUF = dat << 8;         				/* Transmit Byte */
    	SpiaRegs.SPITXBUF = dat << 8;
    	/* while(SpiaRegs.SPISTS.bit.INT_FLAG != 1); */ 	/* Wait until the RXBUF has received last bit */
    	asm(" nop");
    	asm(" nop");
    	while(SpiaRegs.SPISTS.bit.INT_FLAG != 1);
    	asm(" nop");
    	asm(" nop");
    	  														/* Read Byte from RXBUF and return */
    
    
    	/**/
    
    	/*while(Spi_Regs->SPISTS.bit.INT_FLAG != 1); 	//Wait until the RXBUF has received last bit
    	asm(" nop");
    	asm(" nop");
    	rxdatabuf[rx_index] = Spi_Regs->SPIRXBUF;
    	rx_index++;
      	return rxdatabuf[rx_index-1];			//Read Byte from RXBUF and return*/
    
    	/**/
    }
    
    
    /*-----------------------------------------------------------------------*/
    /* Receive a byte from MMC via SPI  (Platform dependent)                 */
    /*-----------------------------------------------------------------------*/
    
    static
    BYTE rcvr_spi (void)
    {
    //    DWORD rcvdat;
    //
    //    SPIDataPut(&SpiaRegs, 0xFF); /* write dummy data */
    //
    //    SPIDataGet(&SpiaRegs, (unsigned int *) &rcvdat); /* read data frm rx fifo */
    //
    //    return (BYTE)rcvdat;
    	/*return spi_xmit(&SpiaRegs, 0xFF << 8);*/
    
    	BYTE ret;
      	SpiaRegs.SPITXBUF = 0xFF;        				/* Transmit DUMMY Byte */
    	while(SpiaRegs.SPISTS.bit.INT_FLAG == 0){}; 	/* Wait until the RXBUF has received last bit */
    	ret = (SpiaRegs.SPIRXBUF);						/*Read Byte from RXBUF and return */
    	return ret;
    
    
    
    }
    
    
    static
    void rcvr_spi_m (BYTE *dst)
    {
        *dst = rcvr_spi();
    }
    
    /*-----------------------------------------------------------------------*/
    /* Wait for card ready                                                   */
    /*-----------------------------------------------------------------------*/
    
    static
    BYTE wait_ready (void)
    {
        BYTE res;
    
    
        Timer2 = 50;    /* Wait for ready in timeout of 500ms */
        rcvr_spi();
        do
            res = rcvr_spi();
        while ((res != 0xFF) && Timer2);
    
        return res;
    }
    
    /*-----------------------------------------------------------------------*/
    /* Send 80 or so clock transitions with CS and DI held high. This is     */
    /* required after card power up to get it into SPI mode                  */
    /*-----------------------------------------------------------------------*/
    static
    void send_initial_clock_train (void)
    {
        unsigned int i;
        DWORD dat;
    
        /* Ensure CS is held high. */
        DESELECT();
    
        /* Switch the SSI TX line to a GPIO and drive it high too. */
    //    GPIOPinTypeGPIOOutput(SDC_GPIO_PORT_BASE, SDC_SSI_TX);
    //    GPIOPinWrite(SDC_GPIO_PORT_BASE, SDC_SSI_TX, SDC_SSI_TX);
    
        /* Send 10 bytes over the SSI. This causes the clock to wiggle the */
        /* required number of times. */
        for(i = 0 ; i < 10 ; i++)
        {
            /* Write DUMMY data. SSIDataPut() waits until there is room in the */
            /* FIFO. */
    		rcvr_spi();
    
        }
    
        /* Revert to hardware control of the SSI TX line. */
    //    GPIOPinTypeSSI(SDC_GPIO_PORT_BASE, SDC_SSI_TX);
    }
    
    /*-----------------------------------------------------------------------*/
    /* Power Control  (Platform dependent)                                   */
    /*-----------------------------------------------------------------------*/
    /* When the target system does not support socket power control, there   */
    /* is nothing to do in these functions and chk_power always returns 1.   */
    
    static
    void power_on (void)
    {
    
    	unsigned int test;
        /*
         * This doesn't really turn the power on, but initializes the
         * SSI port and pins needed to talk to the card.
         */
    
         //EALLOW;
    
        /* Enable the peripherals used to drive the SDC on SPI */
    
    	//SysCtrlRegs.PCLKCR0.bit.SPIAENCLK = 1;
    
    
        /*
         * Configure the appropriate pins to be SSI instead of GPIO. The CS
         * signal is directly driven to ensure that we can hold it low through a
         * complete transaction with the SD card.
         */
         //TODO: Board Specific Pin Configuration
         //GPIO54 - MOSI - PER1
         //GPIO55 - MISO - PER1
         //GPIO56 - CLK - PER1
         //GPIO57 - CS - GPIO
         /*GpioCtrlRegs.GPBMUX2.bit.GPIO54 = 1;
         GpioCtrlRegs.GPBDIR.bit.GPIO54 = 1;
         //GpioCtrlRegs.GPBQSEL2.bit.GPIO54 = 3;
    
         GpioCtrlRegs.GPBMUX2.bit.GPIO55 = 1;
         GpioCtrlRegs.GPBDIR.bit.GPIO55 = 0;
         GpioCtrlRegs.GPBQSEL2.bit.GPIO55 = 3;
    
         GpioCtrlRegs.GPBMUX2.bit.GPIO56 = 1;
         GpioCtrlRegs.GPBDIR.bit.GPIO56 = 1;
         //GpioCtrlRegs.GPBQSEL2.bit.GPIO56 = 3;
    
         GpioCtrlRegs.GPBMUX2.bit.GPIO57 = 0;
         GpioCtrlRegs.GPBDIR.bit.GPIO57 = 1;
         //GpioCtrlRegs.GPBQSEL2.bit.GPIO57 = 3;
         //CS High
         GpioDataRegs.GPBDAT.bit.GPIO57 = 1;*/
    
    
    //     GpioDataRegs.GPBDAT.bit.GPIO54 = 1;
    //     GpioDataRegs.GPBDAT.bit.GPIO55 = 1;
    //     GpioDataRegs.GPBDAT.bit.GPIO56 = 1;
    //     GpioDataRegs.GPBDAT.bit.GPIO57 = 1;
    //     GpioDataRegs.GPBDAT.bit.GPIO54 = 0;
    //     GpioDataRegs.GPBDAT.bit.GPIO55 = 0;
    //     GpioDataRegs.GPBDAT.bit.GPIO56 = 0;
    //     GpioDataRegs.GPBDAT.bit.GPIO57 = 0;
    
        /* Deassert the SSI0 chip selects for both the SD card and serial flash */
    //    GPIOPinWrite(SDCARD_CS_BASE, SDCARD_CS_PIN, SDCARD_CS_PIN);
    //    GPIOPinWrite(SFLASH_CS_BASE, SFLASH_CS_PIN, SFLASH_CS_PIN);
    
        /* Configure the SSI0 port */
        //SysCtrlRegs.LOSPCP.all = 0;
        //SpiaRegs.SPIBRR = 0;
    
        //InitSpi(&SpiaRegs, SPI_CR_SW_RESET | SPI_CR_CHAR_8 | SPI_CR_CLKPOL_RIS, SPI_CTL_MASTER | SPI_CTL_TALK, 0);
        //InitSpi(&SpiaRegs, SPI_CR_SW_RESET | SPI_CR_CHAR_8 | SPI_CR_CLKPOL_FAL, SPI_CTL_MASTER | SPI_CTL_TALK, 0);
        //InitSpi(&SpiaRegs,  SPI_CR_SW_RESET | SPI_CR_CHAR_8 | SPI_CR_CLKPOL_RIS, SPI_CTL_MASTER | SPI_CTL_TALK | SPI_CTL_CLKPHS_90, 0x7F);
    
        InitSpi();
    
        //InitSpi(&SpiaRegs, SPI_CR_SW_RESET | SPI_CR_CHAR_8 | SPI_CR_CLKPOL_FAL, SPI_CTL_MASTER | SPI_CTL_TALK | SPI_CTL_CLKPHS_90, 0);
        //TODO: Set bit rate
        //No divide on low speed clock
    
    
    
    //    SSIConfigSetExpClk(SDC_SSI_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
    //                       SSI_MODE_MASTER, 400000, 8);
    //    SSIEnable(SDC_SSI_BASE);
    
        /* Set DI and CS high and apply more than 74 pulses to SCLK for the card */
        /* to be able to accept a native command. */
        send_initial_clock_train();
    
        PowerFlag = 1;
    }
    
    // set the SSI speed to the max setting
    static
    void set_max_speed(void)
    {
        unsigned long i;
    
        /* Disable the SSI */
    //    SSIDisable(SDC_SSI_BASE);
    
        /* Set the maximum speed as half the system clock, with a max of 12.5 MHz. */
    //    i = SysCtlClockGet() / 2;
        if(i > 12500000)
        {
            i = 12500000;
        }
    
        SpiaRegs.SPIBRR =0x0030;
    
        /* Configure the SSI0 port */
    //    SSIConfigSetExpClk(SDC_SSI_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
    //                       SSI_MODE_MASTER, i, 8);
    
        /* Enable the SSI */
    //    SSIEnable(SDC_SSI_BASE);
    }
    
    static
    void power_off (void)
    {
        PowerFlag = 0;
    }
    
    static
    int chk_power(void)        /* Socket power state: 0=off, 1=on */
    {
        return PowerFlag;
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Receive a data packet from MMC                                        */
    /*-----------------------------------------------------------------------*/
    
    static
    Uint16 rcvr_datablock (
        BYTE *buff,            /* Data buffer to store received data */
        UINT btr            /* Byte count (must be even number) */
    )
    {
        BYTE token;
    
    
        Timer1 = 10;
        do {                            /* Wait for data packet in timeout of 100ms */
            token = rcvr_spi();
        } while ((token == 0xFF) && Timer1);
        if(token != 0xFE) return 0;    /* If not valid data token, retutn with error */
    
        do {                            /* Receive the data block into buffer */
            rcvr_spi_m(buff++);
            rcvr_spi_m(buff++);
        } while (btr -= 2);
        rcvr_spi();                        /* Discard CRC */
        rcvr_spi();
    
        return 1;                    /* Return with success */
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Send a data packet to MMC                                             */
    /*-----------------------------------------------------------------------*/
    
    #if _READONLY == 0
    static
    Uint16 xmit_datablock (
        const BYTE *buff,    /* 512 byte data block to be transmitted */
        BYTE token            /* Data/Stop token */
    )
    {
        BYTE resp, wc;
    
    
        if (wait_ready() != 0xFF) return 0;
    
        xmit_spi(token);                    /* Xmit data token */
        if (token != 0xFD) {    /* Is data token */
            wc = 0;
            do {                            /* Xmit the 512 byte data block to MMC */
                xmit_spi(*buff++);
                xmit_spi(*buff++);
            } while (--wc);
            xmit_spi(0xFF);                    /* CRC (Dummy) */
            xmit_spi(0xFF);
            resp = rcvr_spi();                /* Reveive data response */
            if ((resp & 0x1F) != 0x05)        /* If not accepted, return with error */
                return 0;
        }
    
        return 1;
    }
    #endif /* _READONLY */
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Send a command packet to MMC                                          */
    /*-----------------------------------------------------------------------*/
    
    static
    BYTE send_cmd (
        BYTE cmd,        /* Command byte */
        DWORD arg        /* Argument */
    )
    {
        BYTE n, res = 0x00;
    
    
        if (wait_ready() != 0xFF) return 0xFF;
    
        /* Send command packet */
        xmit_spi(cmd);                        /* Command */
        xmit_spi((BYTE)(arg >> 24));        /* Argument[31..24] */
        xmit_spi((BYTE)(arg >> 16));        /* Argument[23..16] */
        xmit_spi((BYTE)(arg >> 8));            /* Argument[15..8] */
        xmit_spi((BYTE)arg);                /* Argument[7..0] */
        //n = 0;
        n = 0xff;
    
    
        if (cmd == CMD0) n = 0x95;            /* CRC for CMD0(0) */
        if (cmd == CMD8) n = 0x87;            /* CRC for CMD8(0x1AA) */
        xmit_spi(n);
    
        /* Receive command response */
        if (cmd == CMD12) rcvr_spi();        /* Skip a stuff byte when stop reading */
        n = 10;                                /* Wait for a valid response in timeout of 10 attempts */
        do
            res = rcvr_spi();
        while ((res & 0x80) && --n);
    
        return res;            /* Return with the response value */
    }
    
    
    
    /*--------------------------------------------------------------------------
    
       Public Functions
    
    ---------------------------------------------------------------------------*/
    
    
    /*-----------------------------------------------------------------------*/
    /* Initialize Disk Drive                                                 */
    /*-----------------------------------------------------------------------*/
    
    DSTATUS disk_initialize (
        BYTE drv        /* Physical drive nmuber (0) */
    )
    {
        BYTE n, ty, ocr[4];
    
    
        if (drv) return STA_NOINIT;            /* Supports only single drive */
        if (Stat & STA_NODISK) return Stat;    /* No card in the socket */
    
        power_on();                            /* Force socket power on */
        send_initial_clock_train();
    
        SELECT();                /* CS = L */
        ty = 0;
        if (send_cmd(CMD0, 0) == 1) {            /* Enter Idle state */
            Timer1 = 100;                        /* Initialization timeout of 1000 msec */
            if (send_cmd(CMD8, 0x1AA) == 1) {    /* SDC Ver2+ */
                for (n = 0; n < 4; n++) ocr[n] = rcvr_spi();
                if (ocr[2] == 0x01 && ocr[3] == 0xAA) {    /* The card can work at vdd range of 2.7-3.6V */
                    do {
                        if (send_cmd(CMD55, 0) <= 1 && send_cmd(CMD41, 1UL << 30) == 0)    break;    /* ACMD41 with HCS bit */
                    } while (Timer1);
                    if (Timer1 && send_cmd(CMD58, 0) == 0) {    /* Check CCS bit */
                        for (n = 0; n < 4; n++) ocr[n] = rcvr_spi();
                        ty = (ocr[0] & 0x40) ? 6 : 2;
                    }
                }
            } else {                            /* SDC Ver1 or MMC */
                ty = (send_cmd(CMD55, 0) <= 1 && send_cmd(CMD41, 0) <= 1) ? 2 : 1;    /* SDC : MMC */
                do {
                    if (ty == 2) {
                        if (send_cmd(CMD55, 0) <= 1 && send_cmd(CMD41, 0) == 0) break;    /* ACMD41 */
                    } else {
                        if (send_cmd(CMD1, 0) == 0) break;                                /* CMD1 */
                    }
                } while (Timer1);
                if (!Timer1 || send_cmd(CMD16, 512) != 0)    /* Select R/W block length */
                    ty = 0;
            }
        }
        CardType = ty;
        DESELECT();            /* CS = H */
        rcvr_spi();            /* Idle (Release DO) */
    
        if (ty) {            /* Initialization succeded */
            Stat &= ~STA_NOINIT;        /* Clear STA_NOINIT */
            set_max_speed();
        } else {            /* Initialization failed */
            power_off();
        }
    
        return Stat;
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Get Disk Status                                                       */
    /*-----------------------------------------------------------------------*/
    
    DSTATUS disk_status (
        BYTE drv        /* Physical drive nmuber (0) */
    )
    {
        if (drv) return STA_NOINIT;        /* Supports only single drive */
        return Stat;
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Read Sector(s)                                                        */
    /*-----------------------------------------------------------------------*/
    
    DRESULT disk_read (
        BYTE drv,            /* Physical drive nmuber (0) */
        BYTE *buff,            /* Pointer to the data buffer to store read data */
        DWORD sector,        /* Start sector number (LBA) */
        BYTE count            /* Sector count (1..255) */
    )
    {
        if (drv || !count) return RES_PARERR;
        if (Stat & STA_NOINIT) return RES_NOTRDY;
    
        if (!(CardType & 4)) sector *= 512;    /* Convert to byte address if needed */
    
        SELECT();            /* CS = L */
    
        if (count == 1) {    /* Single block read */
            if ((send_cmd(CMD17, sector) == 0)    /* READ_SINGLE_BLOCK */
                && rcvr_datablock(buff, 512))
                count = 0;
        }
        else {                /* Multiple block read */
            if (send_cmd(CMD18, sector) == 0) {    /* READ_MULTIPLE_BLOCK */
                do {
                    if (!rcvr_datablock(buff, 512)) break;
                    buff += 512;
                } while (--count);
                send_cmd(CMD12, 0);                /* STOP_TRANSMISSION */
            }
        }
    
        DESELECT();            /* CS = H */
        rcvr_spi();            /* Idle (Release DO) */
    
        return count ? RES_ERROR : RES_OK;
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Write Sector(s)                                                       */
    /*-----------------------------------------------------------------------*/
    
    #if _READONLY == 0
    DRESULT disk_write (
        BYTE drv,            /* Physical drive nmuber (0) */
        const BYTE *buff,    /* Pointer to the data to be written */
        DWORD sector,        /* Start sector number (LBA) */
        BYTE count            /* Sector count (1..255) */
    )
    {
        if (drv || !count) return RES_PARERR;
        if (Stat & STA_NOINIT) return RES_NOTRDY;
        if (Stat & STA_PROTECT) return RES_WRPRT;
    
        if (!(CardType & 4)) sector *= 512;    /* Convert to byte address if needed */
    
        SELECT();            /* CS = L */
    
        if (count == 1) {    /* Single block write */
            if ((send_cmd(CMD24, sector) == 0)    /* WRITE_BLOCK */
                && xmit_datablock(buff, 0xFE))
                count = 0;
        }
        else {                /* Multiple block write */
            if (CardType & 2) {
                send_cmd(CMD55, 0); send_cmd(CMD23, count);    /* ACMD23 */
            }
            if (send_cmd(CMD25, sector) == 0) {    /* WRITE_MULTIPLE_BLOCK */
                do {
                    if (!xmit_datablock(buff, 0xFC)) break;
                    buff += 512;
                } while (--count);
                if (!xmit_datablock(0, 0xFD))    /* STOP_TRAN token */
                    count = 1;
            }
        }
    
        DESELECT();            /* CS = H */
        rcvr_spi();            /* Idle (Release DO) */
    
        return count ? RES_ERROR : RES_OK;
    }
    #endif /* _READONLY */
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Miscellaneous Functions                                               */
    /*-----------------------------------------------------------------------*/
    
    DRESULT disk_ioctl (
        BYTE drv,        /* Physical drive nmuber (0) */
        BYTE ctrl,        /* Control code */
        void *buff        /* Buffer to send/receive control data */
    )
    {
        DRESULT res;
        BYTE n, csd[16], *ptr = buff;
        WORD csize;
    
    
        if (drv) return RES_PARERR;
    
        res = RES_ERROR;
    
        if (ctrl == CTRL_POWER) {
            switch (*ptr) {
            case 0:        /* Sub control code == 0 (POWER_OFF) */
                if (chk_power())
                    power_off();        /* Power off */
                res = RES_OK;
                break;
            case 1:        /* Sub control code == 1 (POWER_ON) */
                power_on();                /* Power on */
                res = RES_OK;
                break;
            case 2:        /* Sub control code == 2 (POWER_GET) */
                *(ptr+1) = (BYTE)chk_power();
                res = RES_OK;
                break;
            default :
                res = RES_PARERR;
            }
        }
        else {
            if (Stat & STA_NOINIT) return RES_NOTRDY;
    
            SELECT();        /* CS = L */
    
            switch (ctrl) {
            case GET_SECTOR_COUNT :    /* Get number of sectors on the disk (DWORD) */
                if ((send_cmd(CMD9, 0) == 0) && rcvr_datablock(csd, 16)) {
                    if ((csd[0] >> 6) == 1) {    /* SDC ver 2.00 */
                        csize = csd[9] + ((WORD)csd[8] << 8) + 1;
                        *(DWORD*)buff = (DWORD)csize << 10;
                    } else {                    /* MMC or SDC ver 1.XX */
                        n = (csd[5] & 15) + ((csd[10] & 128) >> 7) + ((csd[9] & 3) << 1) + 2;
                        csize = (csd[8] >> 6) + ((WORD)csd[7] << 2) + ((WORD)(csd[6] & 3) << 10) + 1;
                        *(DWORD*)buff = (DWORD)csize << (n - 9);
                    }
                    res = RES_OK;
                }
                break;
    
            case GET_SECTOR_SIZE :    /* Get sectors on the disk (WORD) */
                *(WORD*)buff = 512;
                res = RES_OK;
                break;
    
            case CTRL_SYNC :    /* Make sure that data has been written */
                if (wait_ready() == 0xFF)
                    res = RES_OK;
                break;
    
            case MMC_GET_CSD :    /* Receive CSD as a data block (16 bytes) */
                if (send_cmd(CMD9, 0) == 0        /* READ_CSD */
                    && rcvr_datablock(ptr, 16))
                    res = RES_OK;
                break;
    
            case MMC_GET_CID :    /* Receive CID as a data block (16 bytes) */
                if (send_cmd(CMD10, 0) == 0        /* READ_CID */
                    && rcvr_datablock(ptr, 16))
                    res = RES_OK;
                break;
    
            case MMC_GET_OCR :    /* Receive OCR as an R3 resp (4 bytes) */
                if (send_cmd(CMD58, 0) == 0) {    /* READ_OCR */
                    for (n = 0; n < 4; n++)
                        *ptr++ = rcvr_spi();
                    res = RES_OK;
                }
    
    //        case MMC_GET_TYPE :    /* Get card type flags (1 byte) */
    //            *ptr = CardType;
    //            res = RES_OK;
    //            break;
    
            default:
                res = RES_PARERR;
            }
    
            DESELECT();            /* CS = H */
            rcvr_spi();            /* Idle (Release DO) */
        }
    
        return res;
    }
    
    
    
    /*-----------------------------------------------------------------------*/
    /* Device Timer Interrupt Procedure  (Platform dependent)                */
    /*-----------------------------------------------------------------------*/
    /* This function must be called in period of 10ms                        */
    
    void disk_timerproc (void)
    {
    
    	//BYTE pv, s;
        BYTE n;
    
    
        n = Timer1;                        /* 100Hz decrement timer */
        if (n) Timer1 = --n;
        n = Timer2;
        if (n) Timer2 = --n;
    
        /**/
       /* n = pv;
        pv = SOCKPORT & (SOCKWP | SOCKINS);    // Sample socket switch
    
        if(n == pv) {                    // Have contacts stabled?
        	s = Stat;
    		if (pv & SOCKWP)            // WP is H (write protected)
    		  s |= STA_PROTECT;
    		else                        // WP is L (write enabled)
    			s &= ~STA_PROTECT;
    
            if (pv & SOCKINS)            // INS = H (Socket empty)
                s |= (STA_NODISK | STA_NOINIT);
            else                        // INS = L (Card inserted)
                s &= ~STA_NODISK;
    
            Stat = s;
         }*/
    
    
    }
    
    /*---------------------------------------------------------*/
    /* User Provided Timer Function for FatFs module           */
    /*---------------------------------------------------------*/
    /* This is a real time clock service to be called from     */
    /* FatFs module. Any valid time must be returned even if   */
    /* the system does not support a real time clock.          */
    
    DWORD get_fattime (void)
    {
    
        return    ((2013UL-1980) << 25)    // Year = 2013
                | (10UL << 21)            // Month = October
                | (17UL << 16)            // Day = 17
                | (14U << 11)            // Hour = 14
                | (24U << 5)            // Min = 24
                | (0U >> 1)                // Sec = 0
                ;
    
    }