Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I am willing to store operational parameters, which could be updated over UART on an F28069 Piccolo ControlStick.
I tried Flash API utility from ControlSuite TMS320F2806x Flash API V1.00 release1.1. Could not succeed to review written memory values in debugger. I've used Example_Flash2806x_API.c (31Mar2011). Frequency test with pin34 toggle, I've measured 20kHz (reported to set 10kHz). I didnot change any parameters in the given code. Any advise?
I also have another resource: EEPROM Emulation With the TMS320F28xxx DSCs -SPRAB69. Didnot try this fileset, it was outdated (2009). Should I completely forget about this document?
Which way should I follow to store a bunch of variable bytes in F28069 nonvolatile memory?
Regards,
AdnanKurt