This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Symmetric HRPWM possible?

Hi all,

is symmetric High resolution PWM (HRPWM) with MEP possible?

It is not obvious from the datasheet, but if I set EpwmRegs.EDGMODE = 3 (MEP control of both edges), CMPAHR has no effect any more.

I can do symmetric PWM with EDGMODE=1 or 2 (only on rising or falling edge), but then there is a "gap" between CMPA=x, CMPAHR=0xFF00 and CMPA=x+1, CMPAHR=0.

The datasheet says "EDGMODE=3: MEP control of both edges (TBPHSHR or TBPRDHR)" - this may imply that it does not work for HRPWM, only for HR phase shift and HR period.

  • Stephan,

    What device are you using?

    The 2802x and 2803x devices allow for high-resolution symmetric HRPWM with (TBPRDHR+CMPAHR) or with TBPHSHR.

    The 2833x, 2823x, 280x, and 2804x devices allow for high-resolution HRPWM in symmetric mode only with TBPHSHR.

    In all of the above cases, EDGMODE = 3.

    CMPAHR = 0xFF00 is not necessarily the maximum number of MEP steps in a SYSCLK cycle. You have to scale by the MEP_ScaleFactor (# of MEP steps per sysclk cycle changes by Vdd and temperature).  Please see the HRPWM reference guide for more information OR see the hrpwm_sfo examples that come with the header files and peripheral examples.

     

  • I am using the 28035.

    So it should be possible - then there must be something wrong with my configuration.

    I just wanted to have this confirmed since datasheet AND examples are not handling symmetric duty cycle, only symmetric period.

  • Now I have tried to change the "hrpwm_duty_sfo_v6" example to symmetric PWM and again get no HRPWM.

    The things I changed in the example are all in void HRPWM_Config(period):

    //    (*ePWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UP;
        (*ePWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;

        //(*ePWM[j]).AQCTLA.bit.ZRO = AQ_SET;               // PWM toggle high/low
        //(*ePWM[j]).AQCTLA.bit.CAU = AQ_CLEAR;
        (*ePWM[j]).AQCTLA.bit.CAU = AQ_SET;
        (*ePWM[j]).AQCTLA.bit.CAD = AQ_CLEAR;

        //(*ePWM[j]).HRCNFG.bit.EDGMODE = HR_FEP;          // MEP control on falling edge
        (*ePWM[j]).HRCNFG.bit.EDGMODE = HR_BEP;          // MEP control on both edges

    Is there something missing?

  • Stefan -

    The  hrpwm_duty_sfo_v6 is single-edge duty high-res control with CMPA:CMPAHR only.

    In symmetric mode, you can only have High-Res. phase or high-res period.  In high-res period mode, you can modify your duty cycle as desired as well.

    Use the hrpwm_prdupdown_sfo_v6 function for symmetric mode and modify this example for duty cycle.  This should be what you are looking for.

  • Ah, enabling high-res period for symmetric pwm (even for high-res duty cycle, not only for high-res period) was the key. Now it works, thanks for the help!