I'm using the TMDS2MTRPFCKIT and Piccolo F2803x control card with F28035 to run the project of LVMultiAxis+PfcKit_v1.4-2xPM_Sensorless.
Because of the memory mapping problem, I can not run the program at RAM configuration. But when I tried to run the program on CCS5.3.0 in FLASH configuration, I met some problems about observing the datalog graph. On build LEVEL 1, the graph of datalog buffer is always zero, even though I can see the variables of DlogCh# are changing from the watch window and the correct waveform of the output from the low pass filter.
Moreover, when I tested build LEVEL2 the graph of datalog is still zero and I cannot get the correct waveform from the current test points. And my configuration of the graph window is just like the one in HowToRunGuidev1.1.
Yuan