Other Parts Discussed in Thread: TMS320F28335, UNIFLASH
Greetings ...!!!!
I use the following for my embedded system development.
Delfino experimenter kit - TMS320F28335
Code composer studio - CCSV4
Matlab - 2011b
The issue is in programming the flash memory..!!!
I have changed the "target preference setting" in Matlab for flash programming.
Once I generate the code, the Matlab command window says - "the build is done, but error in downloading".
I could find my .out file and load them in ccsv4.
While the programming is being loaded, i could see at the bottom left - say like a operation progress status -
" erasing the Flash sector" - "loading the program and all"
Then I run the program and it works.The program is simple led blinking on the control card itself.
But it doesn't work once I power Off and On the controller.
Kindly, help me out..
Kind Regards
Karuna