Hello.
I control EPWM and ADC interrupt. pair channel one and pair channel 2,3,4 are independent.
after finishing channel one pulse . channel 2,3,4 turn on.
and channel 4 falling edge is connected with interrupt. in that interrupt ADC conversion will start
so register should be changed to control EPWM.
at the first time when debugging the code, channel 4 interrupt perfectly work. after that I change the EPWM register
second time when turn on the channel 2,3,4 again, EPWM4 channel interrupt is ignored by something.
help me. ;(