I have another repeating XRS pulse output from the processor problem. This processor was programmed and running but we detected a problem with our power supply not putting out our 20V and +/-15V supply voltages properly so we replaced the transformer. Now all the supplies are good but the processor is doing constant resets through the XRS pin. This all started because we have 9 units that all are measuring erratic periods on eCAP1. We have an older unit that is perfect.
I have attached 3 oscilloscope plots that show the resets are 5us pulses occurring every 10us continuing for 150us to 175us in duration and repeating every 29.3ms.
My objective is to narrow the source of the problem down from 100 pins to something less. ;^)
Thanks in advance.