This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: VDD, VDDA



Hi All,

I'm having a question about the voltage supplies of the TMS320F28377.

Are VDD and VDDA internally connected together or are they different (isolated) supply rails.

best regards,

Tjarco

  • Hi Tjarco,

    VDD is actually 1.2V while VDDA is 3.3V. 

    There are a few more 3.3V rails too:

    VDDIO: (I/O supplies)

    VDD3VFL: (Flash supply)

    VDDOSC: Oscillator supply

    I am not sure to what extent these supplies are isolated from each other, but you should tie all the supplies together, with separate decoupling capacitors on each pin, and power up these 3.3V rails together.

  • Hi Devin,

    Yes sorry, I mend the VDD3VFL, VDDA, VDDIO and VDDOSC. Is the VDDA a "isolated" supply rails only for analogue subsystem, or are all these 3V3 supplies internally tied together?

  • Tjarco,

    Yes, these supplies are internally isolated from each other.  This is done primarily for internal noise isolation between the supplies. 

    What is the reason behind the question?  Are you seeing issues or just curiosity?

    Best regards,
    Jason

  • Hi Jason,


    No I'm having separated power supplies for analogue and digital 3V3, but if they we tied together internally then the two supplies would result in currents through the VDD3VFL, VDDA, VDDIO and VDDOSC pins. So I'm glad to hear they're internally isolated.

    Thank you!