Other Parts Discussed in Thread: UNIFLASH
Code Composer Studio (CCS):
- CCS 6.0 (or 6.0.1) and later is required
- Device configuration and flash programming support is available through CCS updates for 6.0 and 6.0.1.
- C28x Compiler: Codegen 6.2.9 or later is highly recommended for all applications.
- Note: Support for TMU, VCU and CLA were introduced in 6.2.4
- Always check CCS updates for the latest version of the compiler, flash programming and device configuration files.
DSP/BIOS:
- Will not be supported.
SYS/BIOS:
- Portions of SYS/BIOS are included in the ROM of this device.
- If you are using the ROM image of SYS/BIOS then you must use 6.37.05
- If you are not using the ROMed image (only flash/RAM), then SYS/BIOS 6.41.00 or later is recommended.
- http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/bios/sysbios/
- http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/rtsc/
- Support for JTAG programming is planned to be integrated Uniflash 3.3 expected in February.
- Serial programming support is planned for 1Q15
ControlSUITE: Available today
- Device support / examples.
PinMUX tool:
- A new, improved tool is available !
- The new tool, which currently supports 2837xD, can be downloaded here: http://www.ti.com/tool/pinmuxtool
- This tool will be updated to include 2837xS and 2807x by end of Dec 2014
- (Note: the pinMUX currently in controlSUITE will not be supported for 2837xD, 2837xS or 2807x).
JTAG Controller Support:
- XDS100v2, XDS200 and XDS510USB, XDS560 supported
- Spectrum Digital XDS510. A patch from Spectrum Digital through Code Composer Studio updates, released in Jan 2014, is required for CLA support.
- Blackhawk USB2000: Requires Blackhawk update available through CCS updates
- Update: Blackhawk released updated drivers on April 18, 2014 that improve programming times. Build 343 of the CCS 5.5 and 6.0 emupacks for BH have this update (v5.5.0.323 and v6.0.0.343 should be listed when you perform updates through Code Composer Studio.
- Will not be supported: Spectrum Digital XDS510LC
Codeskin 3rd party flash programmer:
- Please send any requests for support directly to Codeskin info@codeskin.com