Other Parts Discussed in Thread: TMS320F28377S, TMS320F28377D
There are high speed SPI ports available on the TMS320F28377S which can do a maximum of 40MHz if some design guidelines are met.
Since you can configure a non highspeed SPI rate to be 50MHz (= max rate thru SPIBRR = max LSPCLK/4 = max SYSCLK/4 [default is SYSCLK/16] for a 200MHz SYSCLK), but this contradicts the need for a high speed SPI port which can do max 40MHz with design guidelines and shouldn't be the max speed of a non high speed SPI port.
I found one similar question but the answer is the same contradiction that is in the datasheet. Here they state that any GPIO max freq rate is 50MHz.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/355840
Thanks in advance for the help,
Jason