Other Parts Discussed in Thread: TMS320F28027, CONTROLSUITE
I am using TMS320F28027 launchpad
I want to display text on LCD 16 x2 in 4 bit mode
can u guide me please
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28027, CONTROLSUITE
I am using TMS320F28027 launchpad
I want to display text on LCD 16 x2 in 4 bit mode
can u guide me please
Ashutosh,
Please take a look at this thread, I think the last post should be of some help.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/210923#pi316717=2
Matt
I am surprised that LCD interfacing with tms320f28027 is not possible what are the probable problems
Its not that... "Its not possible!"... its just that its not as easy like we do it with MSP430 or 8-bit Atmel or PIC devices.
This is as close you can get: 
Regards,
Gautam
Dear Gautam,
Please guide me for serial port LCD interface.
Also guide me about programming code for interfacing LCD in serial port.
What you can do is use Serial LCD as mentioned in below link:

Use this sample code to communicate with the LCD: sci_echoback
C:\ti\controlSUITE\device_support\f2802x\v129\DSP2802x_examples_ccsv4\sci_echoback
Regards,
Gautam
Dear
My attempt to run Launcpad with 16x2 LCD (+5Volt) in 4bit mode led to sudden disaster
Last two three days Whenever I used to run program the LCD used to clear the screen But never use to show the text.
However, suddenly today there was short circuit ,
which has led to damage of my PC USB port, also launchpad and the power supply (5Volt regulator used to drive LCD).
I had connected the Power ground and Launchpad ground.
Also since the LCD may ouput the busy flag at D7 pin which may be 5 Volt, so I never used my controller in read mode. instead i used delay to confrim LCD is free.
After making several attempts how suddenly it has happened like this.
What must have happened.
Please suggest the possible reasons.
Are these repaired by Ti or any distributor please let me know.
Or any other agencies are there who repair such boards
Or they use and throw.
I feel that Fuse F1 and Regulator (3.3volt) U4 is been damaged. Other components I am not sure.
How to confirm all these things.
As the components are SMD devices They are very difficult to debug.
Yesterday I tried to purchase from TI store but they are now saying 17.05$ +7 $ ( shipping) also when I click on checkout they say 17.05$+20$( shipping), why they are doing so.
As three months when I had purchased They hadnt charged me any shipping charges I had purchased only in 17.05$.