This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External memory not working during FLASH (F28335)



Hi,

 I am using a custom F28335 board with external SRAM (256 kB x16). The off chip SRAM is mapped to Zone 6 (origin=0x100000, length=0x40000).

The size of the variables used in the program is well within the SRAM and FLASH capacity of the board.

When i debug the code in SRAM, the code is working fine. Similarly when i debug the code in FLASH it is also working fine.

But, when i disconnect the DSP board from emulator, the programming is not running in DSP.

I am initializing the external memory in DSP2833x_CodeStartBranch.asm    using  InitExtMemIf

I have got InitExtMemIf. asm () file from my previous post in TI community and have modified it. i have attached the assembly file for reference.

I have done modifications in the InitExtMemIf. asm file based on the value of GPCMUX1, GPCMUX2, GPBMUX1, GPAMUX2 and XTIMING6 given in the gel file.

As the program works well in debug mode, i just used the value present in the gel file to initialize the GPCMUX1, GPCMUX2, GPBMUX1, GPAMUX2 and XTIMING6 in InitExtMemIf. asm file.

Kindly help me in identifying the issue.

Regards,

subash

InitExtMemIf.asm

  • Hi Subash,

    Could you explain a bit more about the flow for your program? What is the use case of SRAM in this case and how the code/data is getting loaded into SRAM?

    I assume you are BOOTING the device from Flash in this case and you have set the BOOTMODE pins appropriately for the same.

    Regards,

    Vivek Singh

  • Hi Vivek Singh,

     i just mapped the .ebss section to  external memory. My .cmd file is as follows,

    MEMORY
    {
    PAGE 0:
        BEGINRAM:     origin=0x0, length=0x2
        RAMM0:     origin=0x2, length=0x3fe
        OTP:     origin=0x380400, length=0x400
        FLASH:     origin=0x300000, length=0x3fff6  (On chip FLASH)
        BEGINFLASH:     origin=0x33fff6, length=0x2
        CSM_PWL:     origin=0x3f7ff8, length=0x8
        IQTABLES:     origin=0x3fe000, length=0xb50
        IQTABLES2:     origin=0x3feb50, length=0x8c
        FPUTABLES:     origin=0x3febdc, length=0x6a0
        ROM:     origin=0x3ff27c, length=0xd44
        RESET:     origin=0x3fffc0, length=0x2
        VECTORS:     origin=0x3fffc2, length=0x3e
        //RAML4L7:     origin=0xc000, length=0x4000
        ADC_CAL:     origin=0x380080, length=0x9
        ZONE7P:     origin=0x100000, length=0x40000  (OFF chip SRAM)
    PAGE 1:
        RAML0L3:      origin=0x8000, length=0x8000
        RAMM1:     origin=0x400, length=0x400
        ZONE7D:     origin=0x210000, length=0x10000
    }
    SECTIONS
    {
        .vectors:     load = 0x000000000
        .text:     > FLASH, PAGE = 0
        .switch:     > FLASH, PAGE = 0
        .bss:     > RAML0L3, PAGE = 1
        .ebss:     > ZONE7P, PAGE = 0
        .far:     > RAML0L3, PAGE = 1
        .cinit:     > FLASH, PAGE = 0
        .pinit:     > FLASH, PAGE = 0
        .const:     > FLASH, PAGE = 0
        .econst:     > FLASH, PAGE = 0
        .reset:     > RESET, PAGE = 0, TYPE = DSECT
        .data:     > RAML0L3, PAGE = 1
        .cio:     > RAML0L3, PAGE = 1
        .sysmem:     > RAML0L3, PAGE = 1
        .esysmem:     > RAML0L3, PAGE = 1
        .stack:     > RAMM1, PAGE = 1
        .rtdx_text:     > FLASH, PAGE = 0
        .rtdx_data:     > RAML0L3, PAGE = 1
        IQmath:     > FLASH, PAGE = 0
        codestart:     > BEGINFLASH, PAGE = 0
        csmpasswds:     > CSM_PWL, PAGE = 0
        csm_rsvd:     > RAMM0, PAGE = 0
        ramfuncs:     LOAD = FLASH,
            RUN = RAMM0,
            LOAD_START(_RamfuncsLoadStart),
            LOAD_END(_RamfuncsLoadEnd),
            RUN_START(_RamfuncsRunStart),
            PAGE = 0
        .adc_cal:     > ADC_CAL, PAGE = 0 , TYPE = NOLOAD
        IQmathTables:     > IQTABLES, PAGE = 0 , TYPE = NOLOAD
        IQmathTables2:     > IQTABLES2, PAGE = 0 , TYPE = NOLOAD
        FPUmathTables:     > FPUTABLES, PAGE = 0 , TYPE = NOLOAD
    }

    The corresponding linker file is as follows,


    MEMORY CONFIGURATION

             name            origin    length      used     unused   attr    fill
    ----------------------  --------  ---------  --------  --------  ----  --------
    PAGE 0:
      BEGINRAM              00000000   00000002  00000000  00000002  RWIX
      RAMM0                 00000002   000003fe  0000001f  000003df  RWIX
      ZONE7P                00100000   00040000  0003eaaa  00001556  RWIX      (length is within the OFF Chip SRAM)
      FLASH                 00300000   0003fff6  00007437  00038bbf  RWIX              (length is within the On Chip FLASH)
      BEGINFLASH            0033fff6   00000002  00000002  00000000  RWIX
      ADC_CAL               00380080   00000009  00000007  00000002  RWIX
      OTP                   00380400   00000400  00000000  00000400  RWIX
      CSM_PWL               003f7ff8   00000008  00000000  00000008  RWIX
      IQTABLES              003fe000   00000b50  00000000  00000b50  RWIX
      IQTABLES2             003feb50   0000008c  00000000  0000008c  RWIX
      FPUTABLES             003febdc   000006a0  00000000  000006a0  RWIX
      ROM                   003ff27c   00000d44  00000000  00000d44  RWIX
      RESET                 003fffc0   00000002  00000000  00000002  RWIX
      VECTORS               003fffc2   0000003e  00000000  0000003e  RWIX

    As you can see the variables sizes are well within the memory. If i run in Debug mode and map the appropriate sections to SRAM, the programming is working fine. If i map the appropriate sections to as FLASH as given above and run in debug mode still it is working. But if i map to FLASH memory and disconnect the emulator it is not working.

    It is something to do with initialization of external memory, but i have already initialized the external memory using the InitExtMemIf.asm in DSP2833x_CodeStartBranch.asm. It is nothing to do with the hardware, as it works fine in both SRAM and FLASH programming when i do not use external SRAM. It is something related to initializing the external RAM when the DSP board is disconnected from emulator. Correct me if i am wrong.

  • There are some tips here for debugging stand-alone code:

    processors.wiki.ti.com/.../FAQs