Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 Defino eMMC support

All:

To add eMMC to an existing Delfino project, should I think about using an interface chip (like the NXP SDIO101A) - it appears that it would match up nicely to the external memory interface of the Delfino products. 

Is this overkill?

eMMC has an 8-bit data bus + CLK + CMD - could this be implemented using the external interface directly, or is the added "host controller" giving some benefit?

(We are interfacing to a 4 GByte eMMC part - and the SPI interface has been "end-of-lifed" so it looks like the 8-bit bus + CLK + CMD is needed...)

  • Hi Todd,

    Couple of questions -

    1) Which Delfino device you are planning to use?

    2) Async Interface may have the CLK but there will not be any timing for Async signals wrt the CLK. Timings will be wrt chip select and the strobes only.

    3) There is no CMD signal in Async Interface? Is this emulated by using GPIO or one of the control signal of Async interface?

    Regards,

    Vivek Singh

     

  • Hi Todd,

    Hope you're doing well. Did you implement the eMMC interface successfully? I've got a customer asking the same questions.

    Regards,
    Mark
  • Mark:
    Just after asking that question, I was moved to a different project. In the end, the decision was made to use the existing technology, which did not involve switching to an eMMC device, so the NXP SDIO101A never got populated onto a board. I think that the newer devices (F28377S & F28377D) have direct support for eMMC, but for older devices like the F28335, I think that the NXP device would work well as a bridge to eMMC.

    Regards,
    Todd Anderson
  • Hi Todd,

    Thanks for the reply. Maybe a good thing you didn't use the SDIO101A. Arrow suggested the SDIO101A is NRND, although I didn't see that noted on the NXP web site.

    Regards,
    Mark