This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Synchronizing DSPs-28335

I need to synchronize 2 DSPs such that they operate exactly in a similar fashion  ( initial delay is acceptable ). These DSPs have to drive 2 inverters which is feeding a motor. The operation of the 2 DSPs are similar. Each DSP will have an internal signal based on which it has to operate. probably timer synchronisation through interrupts is what I am looking for