This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

encodder overflow with motorware lab12b

hello,

my motor max speed is 5000rpm, when motor speed up to 5000rpm, gMotorVars.SpeedQEP_krpm changed to -5.0.

and motor maintained at 5000 rpm, meanwhile, i could not control motor speed by  gMotorVars.SpeedRef_krpm.

system became uncontrolable but hardware did not explosion.

my encoder lines is 16384(USER_MOTOR_ENCODER_LINES = 16384)

and USER_MOTOR_MAX_SPEED_KRPM = 5.0

is there have any overflow or some other problem?

ps:I could not find any real effect on USER_MOTOR_MAX_SPEED_KRPM.