Other Parts Discussed in Thread: ENERGIA
I had installed Energia 0101E0017 but in tools---> board, the board name (Launchxl - F28377s) doesnt appear. what should i do to fix it.
//###########################################################################//// FILE: Example_F28377xLaunchPadDemo.c//// TITLE: F28377S LaunchPad Out of Box Demo//// DESCRIPTION://! \addtogroup f28377xX_example_list//! <h1>Out of Box Demo (LaunchPadDemo)</h1>//!//! This program is the demo program that comes pre-loaded on the F28377S//! LaunchPad development kit. The program starts by flashing the two user//! LEDs. After a few seconds the LEDs stop flashing and the device starts //! sampling ADCIN14 once a second. If the sample is greater than midscale//! the red LED on the board is lit, while if it is lower a blue LED is lit. //! Sample data is also display in a serial terminal via the boards back //! channel UART. You may view this data by configuring a serial termainal //! to the correct COM port at 115200 Baud 8-N-1.//!////###########################################################################// $TI Release: 2837xS C/C++ Header Files V1.00 $// $Release Date: July 15, 2015 $//###########################################################################
#include <stdint.h>#include <stdbool.h>#include <stdio.h>#include <file.h>
#include "F28x_Project.h" // DSP28x Headerfile#include "ti_ascii.h"#include "sci_io.h"
#define CONV_WAIT 1L //Micro-seconds to wait for ADC conversion. Longer than necessary.
extern void DSP28x_usDelay(Uint32 Count);
//static unsigned short indexX=0;//static unsigned short indexY=0;
const unsigned char escRed[] = {0x1B, 0x5B, '3','1', 'm'};const unsigned char escWhite[] = {0x1B, 0x5B, '3','7', 'm'};const unsigned char escLeft[] = {0x1B, 0x5B, '3','7', 'm'};const unsigned char pucTempString[] = "ADCINA0 Sample: ";
///////////////////////////////////////////////////////////////////////////////////////////////////////////////
void ConfigureADC(void);void SetupADCSoftware(void);
//variables to store conversion resultsUint16 AdcaResult0;Uint16 AdcaResult1;Uint16 AdcbResult0;Uint16 AdcbResult1;
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
int16 currentSample_a0;
int16 currentSample_a1;
int16 currentSample_b0;
int16 currentSample_b1;
int16 counter;
Uint16 t_count;
Uint16 spi_data_send;Uint16 spi_data_receive;
/*
int16_t sampleADC_A(void){ int16_t temp; //int16_t temp_b;
//Force start of conversion on SOC0 AdcaRegs.ADCSOCFRC1.all = 0x03;
//start conversions immediately via software, ADCB // AdcbRegs.ADCSOCFRC1.all = 0x03; //SOC0 and SOC1
//Wait for end of conversion. while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0){} //Wait for ADCINT1 AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1
//wait for ADCB to complete, then acknowledge flag // while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0); // AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
//Get temp sensor sample result from SOC0 temp = AdcaResultRegs.ADCRESULT1; // temp_b = AdcbResultRegs.ADCRESULT1;
//Return the raw temperature because the devices don't have slope/offset values return(temp);
}*//*int16_t sampleADC_B(void){ //int16_t temp; int16_t temp_b;
//Force start of conversion on SOC0 //AdcaRegs.ADCSOCFRC1.all = 0x03;
//start conversions immediately via software, ADCB AdcbRegs.ADCSOCFRC1.all = 0x03; //SOC0 and SOC1
//Wait for end of conversion. // while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0){} //Wait for ADCINT1 // AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1
//wait for ADCB to complete, then acknowledge flag while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
//Get temp sensor sample result from SOC0 // temp = AdcaResultRegs.ADCRESULT1; temp_b = AdcbResultRegs.ADCRESULT1;
//Return the raw temperature because the devices don't have slope/offset values return(temp_b);
}*//*void drawTILogo(void){ unsigned char ucChar, lastChar; putchar('\n'); while(indexY<45) { if(indexY<45){ if(indexX<77){ ucChar = ti_ascii[indexY][indexX++] ; //We are in the TI logo make it red if(ucChar != '7' && lastChar=='7'){ putchar(escRed[0]); putchar(escRed[1]); putchar(escRed[2]); putchar(escRed[3]); putchar(escRed[4]); } //We are in the TI logo make it red if(ucChar == '7' && lastChar!='7'){ putchar(escWhite[0]); putchar(escWhite[1]); putchar(escWhite[2]); putchar(escWhite[3]); putchar(escWhite[4]); } putchar(ucChar); lastChar = ucChar; }else{ ucChar = 10; putchar(ucChar); ucChar = 13; putchar(ucChar); indexX=0; indexY++; } } }}*/void clearTextBox(void){
//Change to Red text //putchar(escRed[0]); //putchar(escRed[1]); // putchar(escRed[2]); // putchar(escRed[3]); // putchar(escRed[4]); printf((char*)pucTempString);
}
void updateDisplay(void){ // Restore cursor position printf("\n pin A0 %d \t pin A1 %d \t pin B0 %d\t pin B1 %d \t counter %u \t SPI SENT %u \t SPI RECEIVE %u ",currentSample_a0, currentSample_a1, currentSample_b0, currentSample_b1, t_count, spi_data_send, spi_data_receive); // printf(" \n ADC Sample pin B0 _ 4 %d ", currentSample_b); //printf(" \n ADC Sample pin A1 %d ", 24035); //printf(" \n ADC Sample pin B1 %d ", 14065);}
// SCIA 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parityvoid scia_init(){
// Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function
SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.bit.TXINTENA =1; SciaRegs.SCICTL2.bit.RXBKINTENA =1;
SciaRegs.SCIHBAUD.all =0x0000; // 115200 baud @LSPCLK = 22.5MHz (90 MHz SYSCLK). SciaRegs.SCILBAUD.all =53;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset return;}
//////////////////////////////////////////////////////////////////////////////////////////////////////////////void delay_loop(){ long i; for (i = 0; i < 1000000; i++) {}}
void error(void){ asm(" ESTOP0"); // Test failed!! Stop! for (;;);}
void spi_init(){ SpiaRegs.SPICCR.all =0x000F; // Reset on, rising edge, 16-bit char bits SpiaRegs.SPICTL.all =0x0006; // Enable master mode, normal phase, // enable talk, and SPI int disabled. SpiaRegs.SPIBRR.all =0x007F; SpiaRegs.SPICCR.all =0x009F; // Relinquish SPI from Reset SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission}
void spi_xmit(Uint16 a){ SpiaRegs.SPITXBUF=a;}
void spi_fifo_init(){// Initialize SPI FIFO registers SpiaRegs.SPIFFTX.all=0xE040; SpiaRegs.SPIFFRX.all=0x2044; SpiaRegs.SPIFFCT.all=0x0;}
//===========================================================================// No more.//===========================================================================///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
void main(){ volatile int status = 0; uint16_t i; volatile FILE *fid; ////////////////////////////////////////////////////// Uint16 sdata; // send data Uint16 rdata; // received data
//////////////////////////////////////////////////////
// If running from flash copy RAM only functions to RAM #ifdef _FLASH memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);#endif
// Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2806x_SysCtrl.c file. InitSysCtrl();
// For this example, only init the pins for the SCI-A port. EALLOW; GpioCtrlRegs.GPCMUX2.bit.GPIO84 = 1; GpioCtrlRegs.GPCMUX2.bit.GPIO85 = 1; GpioCtrlRegs.GPCGMUX2.bit.GPIO84 = 1; GpioCtrlRegs.GPCGMUX2.bit.GPIO85 = 1; EDIS;
////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // This example function is found in the F2837xS_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Setup only the GP I/O only for SPI-A functionality // This function is found in F2837xS_Spi.c InitSpiaGpio();
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
// Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT;
// Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2806x_PieCtrl.c file. InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2806x_DefaultIsr.c. // This function is found in F2806x_PieVect.c. InitPieVectTable();
// Initialize SCIA scia_init();
//Initialize GPIOs for the LEDs and turn them off EALLOW; GpioCtrlRegs.GPADIR.bit.GPIO12 = 1; GpioCtrlRegs.GPADIR.bit.GPIO13 = 1; GpioDataRegs.GPADAT.bit.GPIO12 = 1; GpioDataRegs.GPADAT.bit.GPIO13 = 1; EDIS;
// Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM
//Redirect STDOUT to SCI status = add_device("scia", _SSA, SCI_open, SCI_close, SCI_read, SCI_write, SCI_lseek, SCI_unlink, SCI_rename); fid = fopen("scia","w"); freopen("scia:", "w", stdout); setvbuf(stdout, NULL, _IONBF, 0); ///////////////////////////////////////////////////////////////////////////////////////////////////
//spi device peripherals initialisation //Initialize the Device Peripherals: spi_fifo_init(); // Initialize the Spi FIFO spi_init(); // init SPI
///////////////////////////////////////////////////////////////////////////////////////////////////
/* // Configure the ADC: // Initialize the ADC EALLOW;
//write configurations AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE); AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//Set pulse positions to late AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//power up the ADCs AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//delay for 1ms to allow ADC time to power up DELAY_US(1000);*/
/* //ADCA EALLOW; AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin ADCINA0 AdcaRegs.ADCSOC0CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCSOC1CTL.bit.CHSEL = 0; //SOC1 will convert pin ADCINA0 AdcaRegs.ADCSOC1CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared */
/* //ADCB AdcbRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin B0 AdcbRegs.ADCSOC0CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcbRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 will convert pin B1 AdcbRegs.ADCSOC1CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcbRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcbRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared*/
//Print a TI Logo to STDOUT //drawTILogo();
//Twiddle LEDs GpioDataRegs.GPADAT.bit.GPIO12 = 0; GpioDataRegs.GPADAT.bit.GPIO13 = 1;
for(i = 0; i < 50; i++){
GpioDataRegs.GPATOGGLE.bit.GPIO12 = 1; GpioDataRegs.GPATOGGLE.bit.GPIO13 = 1; DELAY_US(50000);
}
//LEDs off GpioDataRegs.GPADAT.bit.GPIO12 = 1; GpioDataRegs.GPADAT.bit.GPIO13 = 1; //Clear out one of the text boxes so we can write more info to it clearTextBox(); //currentSample = 2041; // currentSample_b = sampleADC_B(); //Configure the ADCs and power them up /* ConfigureADC();
//Setup the ADCs for software conversions SetupADCSoftware();
//take conversions indefinitely in loop do { //convert, wait for completion, and store results //start conversions immediately via software, ADCA AdcaRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 //start conversions immediately via software, ADCB AdcbRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 //wait for ADCA to complete, then acknowledge flag while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //wait for ADCB to complete, then acknowledge flag while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //store results AdcaResult0 = AdcaResultRegs.ADCRESULT0; AdcaResult1 = AdcaResultRegs.ADCRESULT1; AdcbResult0 = AdcbResultRegs.ADCRESULT0; AdcbResult1 = AdcbResultRegs.ADCRESULT1;
//at this point, conversion results are stored in //AdcaResult0, AdcaResult1, AdcbResult0, and AdcbResult1
//software breakpoint, hit run again to get updated conversions asm(" ESTOP0");
}while(1); */
//Main program loop - continually sample temperature
counter = 0; t_count = 0;
sdata = 0x0000;
for(;;) { ConfigureADC(); //Setup the ADCs for software conversions
SetupADCSoftware();
//take conversions indefinitely in loop //convert, wait for completion, and store results //start conversions immediately via software, ADCA AdcaRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 //start conversions immediately via software, ADCB AdcbRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1 //wait for ADCA to complete, then acknowledge flag while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //wait for ADCB to complete, then acknowledge flag while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0); AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //store results AdcaResult0 = AdcaResultRegs.ADCRESULT0; AdcaResult1 = AdcaResultRegs.ADCRESULT1; AdcbResult0 = AdcbResultRegs.ADCRESULT0; AdcbResult1 = AdcbResultRegs.ADCRESULT1;
//at this point, conversion results are stored in //AdcaResult0, AdcaResult1, AdcbResult0, and AdcbResult1
//software breakpoint, hit run again to get updated conversions //asm(" ESTOP0");
//Sample ADC currentSample_a0 = (AdcaResult0*8)/10; currentSample_a1 = (AdcaResult1*8)/10; currentSample_b0 = (AdcbResult0*8)/10; currentSample_b1 = (AdcbResult1*8)/10; counter = counter + 1; t_count = t_count + 1;
//Update the serial terminal output updateDisplay(); //If the sample is above midscale light one LED if(currentSample_a0 > 2048){ GpioDataRegs.GPADAT.all = 0x2000; }else{ //Otherwise light the other GpioDataRegs.GPADAT.all = 0x1000; }
//////////////////////////////////////////////////////////////////////////////////////////////////////////////// //spi communication spi_xmit(currentSample_a0); // Wait until data is received while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { } // Check against sent data rdata = SpiaRegs.SPIRXBUF;
spi_data_send = currentSample_a0; spi_data_receive = rdata;
// if(rdata != currentSample_a0) error();
sdata++;
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
//DELAY_US(1); }}
//Write ADC configurations and power up the ADC for both ADC A and ADC Bvoid ConfigureADC(void){ EALLOW;
//write configurations AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE); AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//Set pulse positions to late AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//power up the ADCs AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//delay for 0.5ms to allow ADC time to power up DELAY_US(500);
EDIS;}
void SetupADCSoftware(void){ //Uint16 acqps;
//determine minimum acquisition window (in SYSCLKS) based on resolution /*if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION){ acqps = 14; //75ns } else { //resolution is 16-bit acqps = 63; //320ns }*/
//Select the channels to convert and end of conversion flag //ADCA EALLOW; AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin A0 AdcaRegs.ADCSOC0CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 will convert pin A1 AdcaRegs.ADCSOC1CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared //ADCB AdcbRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin B0 AdcbRegs.ADCSOC0CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcbRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 will convert pin B1 AdcbRegs.ADCSOC1CTL.bit.ACQPS = 25; //sample window is acqps + 1 SYSCLK cycles AdcbRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcbRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared}