Hi,
Please teach me how to program over SCI.
I'm using F28377S LaunchPad and the two projects of the following.
Kernel project:
C:\ti\controlSUITE\device_support\F2837xS\v180\F2837xS_examples_Cpu1\F2837xS_sci_flash_kernel
Download project:
C:\ti\controlSUITE\development_kits\LAUNCHXL-F28377S\LaunchPadDemo
Then I generate hex file as following.

And I tried the program to use the serial flash programmer, but can not be downloaded.
Because the command prompt freezes on the screen of the following.
(C:\ti\controlSUITE\device_support\~Utilities\serial_flash_programmer)
My command of serial flash programmer:
C:\ti\controlSUITE\device_support\~Utilities\serial_flash_programmer>
serial_flash_programmer.exe -d f2837xS -k F2837xS_sci_flash_kernel_cpu01.txt -a Example_28377SLaunchPad.txt -b 38400 -p COM101
Is this my programming flow mistaken?
Best regards,
Mino.M