This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK28027 docking station

Intellectual 630 points

Replies: 2

Views: 324

Which is pin 1 and pin 2 (of the solder-able part of the docking station) so that I can figure out all pin allocations from control suite schematic). Please draw two arrows to indicate pin 1 and pin 2 in photo provided.

Regards,

Amit

2 Replies

  • sorry the photo I provided did not appear. How can I upload it so forum can see it?
  • In reply to Amit Aryal:

    Hi Click on "Use rich Formatting" to get more option. There you can have option to attach files.

    -Aditya

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.