This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buffered UART F28069

 Hi everyone,

I am trying to send data trough UART and since I have a lot of data I tam trying to use a buffered UART. 

I attached the code. For this example I  transmit ASCII characters 1-20 to a terminal. Only 0,1 and 3 are sent  and the Tx interrupt stops after  even if the TXFFINT Flag  is set.

If I increase the TXFFIL to 3  I  0,1,2,3,4 and 5  will be sent   and stop after

Thank you for your help

Hamid

#define FIFO_BUFFER_SIZE 128 // software buffer size (in bytes)

 

void uart_send_byte(Uint8 byte);

 

typedef struct {

  Uint8  data_buf[FIFO_BUFFER_SIZE]; // FIFO buffer

  Uint16 i_first;                    // index of oldest data byte in buffer

  Uint16 i_last;                     // index of newest data byte in buffer

  Uint16 num_bytes;                  // number of bytes currently in buffer

}sw_fifo_typedef;

 

sw_fifo_typedef rx_fifo = { {0}, 0, 0, 0 }; // declare a receive software buffer

sw_fifo_typedef tx_fifo = { {0}, 0, 0, 0 }; // declare a transmit software buffer

volatile Uint8 uart_rx_fifo_not_empty_flag = 0;

volatile Uint8 uart_rx_fifo_full_flag = 0;

volatile Uint8 uart_rx_fifo_ovf_flag = 0;

volatile Uint8 uart_tx_fifo_full_flag = 0;

volatile Uint8 uart_tx_fifo_ovf_flag = 0;

volatile Uint8 uart_tx_fifo_not_empty_flag = 0;

 

main

{

/*

Init code

*/

 

 

 

 

 

 

        // ISR functions found within this file.

           EALLOW;  // This is needed to write to EALLOW protected registers

           PieVectTable.SCIRXINTA = &sciaRxFifoIsr;

           PieVectTable.SCITXINTA = &sciaTxFifoIsr;

           EDIS;   // This is needed to disable write to EALLOW protected registers

           scia_fifo_init();  // Init SCI-A

       

// Enable interrupts required for this example

           PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block

           PieCtrlRegs.PIEIER9.bit.INTx1=1;     // PIE Group 9, INT1

           PieCtrlRegs.PIEIER9.bit.INTx2=1;     // PIE Group 9, INT2

           IER = 0x100; // Enable CPU INT

           EINT;

 

 

 

SciaRegs.SCIFFTX.bit.TXFFIENA=1;

 

 

// transmit ASCII characters 1-20

for(i=0; i<20; i++) {

while(uart_tx_fifo_full_flag);

uart_send_byte(i+48);

}

while(1);

 

}

 

 

 

 

void scia_fifo_init()

{

   SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback

                                  // No parity,8 char bits,

                                  // async mode, idle-line protocol

   SciaRegs.SCICTL1.all =0x0003;  // enable TX, RX, internal SCICLK,

                                  // Disable RX ERR, SLEEP, TXWAKE

 

  SciaRegs.SCICTL2.bit.TXINTENA =1;

 

   SciaRegs.SCICTL2.bit.RXBKINTENA =0;

   SciaRegs.SCIHBAUD = 0x0000;

   SciaRegs.SCILBAUD = SCI_PRD;

   SciaRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back

   SciaRegs.SCIFFTX.all=0xC040;

  // SciaRegs.SCIFFRX.all=0x0022;

   SciaRegs.SCIFFRX.all=0x0022;

 

 

   SciaRegs.SCIFFCT.all=0x00;

 

   SciaRegs.SCICTL1.all =0x0023;     // Relinquish SCI from Reset

   SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;

   SciaRegs.SCIFFRX.bit.RXFIFORESET=1;

 

}

 

 

 

 

 

 

//////////////////////////////////////////////

__interrupt void sciaTxFifoIsr(void) {

//////////////////////////////////////////////

 

 

 

  if(tx_fifo.num_bytes == FIFO_BUFFER_SIZE) { // if the sw buffer is full

    uart_tx_fifo_full_flag = 0;               // clear the buffer full flag because we are about to make room

  }

  if(tx_fifo.num_bytes > 0) {                 // if data exists in the sw buffer

 

         SciaRegs.SCITXBUF = tx_fifo.data_buf[tx_fifo.i_first]; // place oldest data element in the TX hardware buffer

 

    tx_fifo.i_first++;                        // increment the index of the oldest element

    tx_fifo.num_bytes--;                      // decrement the bytes counter

  }

  if(tx_fifo.i_first == FIFO_BUFFER_SIZE) {   // if the index has reached the end of the buffer,

    tx_fifo.i_first = 0;                      // roll over the index counter

  }

  if(tx_fifo.num_bytes == 0) {                // if no more data exists

 

    uart_tx_fifo_not_empty_flag = 0;          // clear flag

 

  

 

 

    SciaRegs.SCIFFTX.bit.TXFFIENA = 0; // disable FIFO interrupts

    SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1; // clear TX FIFO interrupts

 

     PieCtrlRegs.PIEACK.all|=0x100;      // Issue PIE ACK

}

  }

/***************************************************************************************************************/

 

 

void uart_send_byte(Uint8 byte) {

 

  ///////////////////////////////////////////////////////////

  /* disable interrupts while manipulating buffer pointers */

  ///////////////////////////////////////////////////////////

        DINT;                                        // Dnable Global interrupt INTM

 

 

  if(tx_fifo.num_bytes == FIFO_BUFFER_SIZE) {      // no room in the sw buffer

    uart_tx_fifo_ovf_flag = 1;                     // set the overflow flag

  }else if(tx_fifo.num_bytes < FIFO_BUFFER_SIZE) { // if there's room in the sw buffer

    tx_fifo.data_buf[tx_fifo.i_last] = byte;       // transfer data byte to sw buffer

    tx_fifo.i_last++;                              // increment the index of the most recently added element

    tx_fifo.num_bytes++;                           // increment the bytes counter

  }

  if(tx_fifo.num_bytes == FIFO_BUFFER_SIZE) {      // if sw buffer is full

    uart_tx_fifo_full_flag = 1;                    // set the TX FIFO full flag

  }

  if(tx_fifo.i_last == FIFO_BUFFER_SIZE) {         // if the "new data" index has reached the end of the buffer,

    tx_fifo.i_last = 0;                            // roll over the index counter

  }

 

  ///////////////////////

  /* enable interrupts */

  ///////////////////////

  EINT;                                       // Enable Global interrupt INTM

 

  if(tx_fifo.num_bytes > 0) {                      // if there is data in the buffer

 

    uart_tx_fifo_not_empty_flag = 1;               // set flag

 

 

    /* enable UART "TX hw buffer empty" interrupt here                       */

    SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1; // Try and clear the TX FIFO interrupt that gets flagged...

 

SciaRegs.SCIFFTX.bit.TXFFIENA=1;

 

  }

}