Part Number: TMDX28069USB
[Order Number: 936778]
[Part# or Description: TMDX28069USB]
Problem: Order Number: 936778
Type of Help Needed: Need replacement for broken or defective item
Description of Problem:
I Miss Doly Mariyam siddiqui have order four DSP control stick ( TMDX28069USB ). the 4 DSPs received, out of which the 3 of them are not working properly, I am getting error that says fatal error in connecting DSP. I have just started using for my project, only one of them is working properly. when i connected the remaining three, red led was not blinking and when i run the blink led program code, i received fatal error in connecting target and also the f28069 IC was getting heated up and it continued to heat up. One of my friends ordered the DSP, it took 15days for their delivery but when i order the DSP, within 2-3 days i received the DSP for FEDX. Please let me know what can be done, i hope you will rely as soon as possible. its details are as follows
Order Number: 936778
Ordered on: 2/3/2016 7:39:34 AM
Ordered by: DOLY MARIYAM SIDDIQUI
Order Total: 159.96
[Category: eStore]