This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC - No Signal on Output (F28377S LaunchPad)

Using the following configuration code (mostly taken from examples) I am unable to get an output signal on the DAC module.

#include "dac.h"

void InitDAC()
{
	configureDAC(DACA);
}

void configureDAC(Uint16 dac_num)
{
	EALLOW;
	
	CpuSysRegs.PCLKCR16.bit.DAC_A = 1; // enable DAC_A clock

	DacaRegs.DACCTL.bit.DACREFSEL = 1; // use ADC VREFHI instead of an external signal
	DacaRegs.DACCTL.bit.LOADMODE = 0; // load on SysClk not PWMSYNC (PWM not yet enabled)
	DacaRegs.DACOUTEN.bit.DACOUTEN = 1; // enable output
	DacaRegs.DACVALS.all = 0; // output = 0
	DELAY_US(10); // Delay for buffered DAC to power up

	EDIS;
}

/*
 * Sets the DAC's analog voltage based on value
 * Equation:
 * 		With DACVALS = DACVALA = value -->
 * 		VDAC = (DACVALA * DACREF) / 4096  -- spruhx5c.pdf page 1364
 *
 *	With VREFHI from ADC the DACREF value should be 3.3V.
 *	This gives a range for DACVALA of 0 to (4096/3.3) = 1241
 */
void SetDAC(uint16_t DAC, uint16_t value)
{
	DacaRegs.DACVALS.all = value;
	DELAY_US(2);
}

void TestDAC()
{
	uint16_t limit = 1024;
	uint16_t v;
	// ramp up
	for (v = 0; v < limit; v++)
		SetDAC(DACA, v);

	// ramp down
	for (v = limit; v > 0; v--)
		SetDAC(DACA, v);
}

I was unable to locate a possible pin mux configuration, so I'm not sure if that's the issue.  All configuration registers do get their proper values.

I do use InitSysCtrl() from TI's example code as well, so all peripheral clock should be enabled.

main.c contains:

InitDAC();

for(;;)
{
	TestDAC();
	DELAY_US(10);
}

I'm reading my voltages with an oscilloscope from pin J4-32 (also probed DAC2-4 on J4-31, J8-72, J8-71 because there is a naming discrepancy between DAC-A and DAC1).  Is this the correct pin?  What J pin is the ADC VREFHI signal connected to?  I have not checked that reference voltage because I haven't found the pinout.  Switching between VDAC (with a 3.3V reference signal) and ADC VREFHI does not seem to make a difference either.

I would appreciate any insight, thanks!