Hi all.
I have a device created with the TMS320F28016, and now i have not enought memory, so i am using now the TMS320F2802.
I want to migrate the ccv6 project from the old mcu to the new;
* I have configurated all the project details to work with the new mcu.
* I have imported the F2802.cmd and i have indicated the program to use it.
* I have imported the F2802.gel file and i have erased the old one (not indicating the program to use the new one).
I am using the XDS100v2, and i can program correctly the device. But when i want to use it, everything work wrong.
I guess that it is a problem with the memory allocation, but i can't understand what i am doing wrong.
- Where can i indicate the ccv6 to use the new .gel?
- Should i change any other file more than F28016.cmd ->F2802.cmd and F28016.gel->F2802.gel?
- have i got to erase any old file?
-------------------------------------------------
Other thing that happens to me is that when i am using ccv3 with the F28016 mcu everything run ok. But when i use the ccv6 i have to optimize the memory, because the code doesn't fit in memory. But when i do it..... it happens the same than when i use the 2802 mcu... everything work wrong. So now i am using the 28016 mcu with the ccv6 without any memory optimization, and i am eliminating code.......
Any help please ??