I'm trying to compile a project on the C2000 Launchpad f28027.I'm getting a linker error:
warning #10210-D: creating ".esysmem" section with default size of 0x400; use the -heap option to change the default size
"../28027_RAM_lnk.cmd", line 127: error #10099-D: program will not fit into available memory. run placement with alignment/blocking fails for section ".stack" size 0x300 page 1. Available memory ranges:
RAMM1 size: 0x400 unused: 0x0 max hole: 0x0
I am creating a static object, however it should put it in the BSS?
I've already tried adjusting the stack size in Linker properties.
I appreciate any help :)
#include "SomeObject.h" int main(void) { static SomeObject foo; while(1) { if(foo.isReady()) { foo.doWork(); } } }
/* // TI File $Revision: /main/5 $ // Checkin $Date: July 6, 2009 17:18:44 $ //########################################################################### // // FILE: 28027_RAM_lnk.cmd // // TITLE: Linker Command File For 28027 examples that run out of RAM // // This ONLY includes all SARAM blocks on the 28027 device. // This does not include flash or OTP. // // Keep in mind that L0 is protected by the code // security module. // // What this means is in most cases you will want to move to // another memory map file which has more memory defined. // //########################################################################### // $TI Release: DSP2802x Header Files Internal Release 2 $ // $Release Date: July 15, 2008 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\DSP2802x_headers\cmd // // For BIOS applications add: DSP2802x_Headers_BIOS.cmd // For nonBIOS applications add: DSP2802x_Headers_nonBIOS.cmd ========================================================= */ /* ====================================================== // For Code Composer Studio prior to V2.2 // -------------------------------------- // 1) Use one of the following -l statements to include the // header linker command file in the project. The header linker // file is required to link the peripheral structures to the proper // locations within the memory map */ /* Uncomment this line to include file only for non-BIOS applications */ /* -l DSP2802x_Headers_nonBIOS.cmd */ /* Uncomment this line to include file only for BIOS applications */ /* -l DSP2802x_Headers_BIOS.cmd */ /* 2) In your project add the path to <base>\DSP2802x_headers\cmd to the library search path under project->build options, linker tab, library search path (-i). /*========================================================= */ /* Define the memory block start/length for the DSP2802x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F28027 are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. The L0 memory blocks is mirrored - that is it can be accessed in high memory or low memory. For simplicity only one instance is used in this linker file. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ MEMORY { PAGE 0 : /* For this example, L0 is split between PAGE 0 and PAGE 1 */ /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 RAMM0 : origin = 0x000050, length = 0x0003B0 PRAML0 : origin = 0x008000, length = 0x000900 RESET : origin = 0x3FFFC0, length = 0x000002 IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ BOOTROM : origin = 0x3FF27C, length = 0x000D44 PAGE 1 : /* For this example, L0 is split between PAGE 0 and PAGE 1 */ BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ DRAML0 : origin = 0x008900, length = 0x000700 } SECTIONS { /* Setup for "boot to SARAM" mode: The codestart section (found in DSP28_CodeStartBranch.asm) re-directs execution to the start of user code. */ codestart : > BEGIN, PAGE = 0 ramfuncs : > RAMM0 PAGE = 0 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} > RAMM0, PAGE = 0 #endif #endif .text : > PRAML0, PAGE = 0 .cinit : > RAMM0, PAGE = 0 .pinit : > RAMM0, PAGE = 0 .switch : > RAMM0, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMM1, PAGE = 1 .ebss : > DRAML0, PAGE = 1 .econst : > DRAML0, PAGE = 1 .esysmem : > RAMM1, PAGE = 1 IQmath : > PRAML0, PAGE = 0 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNexpTable.obj> (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNasinTable.obj> (IQmathTablesRam) } */ } /* //=========================================================================== // End of file. //=========================================================================== */