Please build the binaries for AT91RM9200 microcontroller.
Now I use ".\SW\bin\OMAP\prime_dc" from "PrimeDC_SDK_PackageV3600"
And there is a problem.
Total nodes ~300. The program crashes after a good work for 2 days:
Sep 30 10:19:31 ucdk Prime Base Node: <COMM_dspKeepAliveRespHndlr> attempts curr<1> / total tx<711>/rx<711> Sep 30 10:19:31 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump ---------------- Sep 30 10:19:31 ucdk Prime Base Node: UTIL_genStackTrace - 1 : [0x41988d94] Sep 30 10:19:31 ucdk Prime Base Node: <UTIL_genStackTrace> -------------------------------------------------
The program works fine and stable if the nodes ~100.