Other Parts Discussed in Thread: TMS320F28335, UNIFLASH
Hi,
Hi i am using TMS320F28335 with ccsv5 and xds100V3 from olimex.
I successfully loaded a toggling program into Flash memory GPIO pins were toggled.
Boot mode was “jump to flash”, all the boot mode pins were high.
Then I was trying to load the same program into Flash memory. But i got an error.
So I erased the flash sectors using uniflash, with boot mode branch to SARAM.
Now no program are loaded in flash.
Then again I loaded the same program into flash successfully, Boot mode was “jump to flash” all the boot mode
pins were high. And GPIO pins were toggled.
Then i was trying to load a program into RAM memory boot mode was branch to SARAM. Suddenly I got the below error, and I could not erase OR unlock the flash sectors.
While loading into RAM I got the below error
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: Breakpoint Manager: Retrying with a AET breakpoint
C28xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x9409: (Error -1066 @ 0x9409) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.232.0)
C28xx: Can't Run Target CPU: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? (Emulation package 5.1.232.0)
C28xx: Trouble Halting Target CPU: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)
C28xx: Error: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Now I could not load the program into flash or ram.
This shows that my devise is locked.
I didn’t interrupt any erasing process, or I didn’t write zero to CSM section.
I read data from password locations using uniflash. 0x33 FFF8 - 0x33 FFFF these locations were zeros.
I have attached the CCS error which I got when I am loading program into ram
How can I solve this issue?
What is the reason for this?
is this this related to boot mode?
I have one more processor, have the same issue.
Thanks in Advance
AKHIL FARNCIS