This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

flash_programming_cpu02 example hangs on SeizeFlashPump() (TMS320F28377D)

Examining the semaphore register shows it is 0.

I've had other difficulties with this example and now have to use tortuous method to download the code. 

I've run the CPU1 version of this code and made sure that the flash semaphore is released.

I've searched the forum for this and it seems that most issues are with custom loaders and not example code.

What do I need to do in order that CPU2 acquire the semaphore? The CPU1 version had no such difficulty.

Thanks!