This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

maximum Vcoclk for TMS320F28096



Hi,

I am using TMS320F28096 with external 20MHz crystal.
In order to have 90MHz for SYSCLK I set up a PLL to *9 /2.

Vcoclk = 20MHz * 9 = 180MHz

SYSCLK = Vcoclk/2 = 90MHz

I found in technical reference that Vcoclk must be at least 50MHz, but what is the maximum limit?
There is no note about that in documentation.

The chip rarely hungs, I want to be sure that PLL is setup correctly, and fequency limit is not exceeded.

Regards,
Piotr