Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE, DRV8301
Tool/software: Code Composer Studio
Hi,
I'm new to CCS, MotorWare, ControlSuite, and the insane amount of documentation. I'm having issues finding the right information to get started for a project that doesn't use TI's BOOST or driver components. I have all the information for motor parameters, driver board specifics, and user I/O. If anyone has some suggestions or tips for getting a project like this set up so that I can plug and play with the modules/API's for the FOC package, that would be great. If this HW is unable to do the suggested tasks, please let me know.
Thanks,
Logan
p.s. Also, I purchased a controlCARD and eval kit just in case it would be easier to work with.
LAUNCHXL-F28068M
interface with pwm to driver board for a IPM motor thats used as an ISG in automotive applications