Other Parts Discussed in Thread: TPS562201
Tool/software: Code Composer Studio
Hi,
Controller- TMS320F28069
Emulator- XDS100V2
My unit has 3 phase Input, It is rectified and given to SMPS (Flyback 120KHz) and 7V DC voltage is generated. This is done in power card. Control Card takes this voltage and generates 3.3V for Controller and JTAG Unit.
Problem:
1. If I Individually power the control card with external DC Supply. The JTAG XDS100V2 works with no problem.
2. When I power the control card with power card, following problems occurs:
a. Sometimes JTAG LED does not glow at all.
b. Sometimes It blinks.
c. Sometimes when LED is ON , while debuggingin CCS, connections gets broken in between randomly and connection is broken.
I have checked the supply from power card and it is clean. There is no issue of current starving, as the complete unit is very well supplied and works well.
Please find below schematic of concerned parts:
Regards,
Siddharth Gupta