This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377 CRC-16 Calculation

Hi

I got the same problem when using f28377 to calculate CRC-16.

Moderator Note: Same problem is referring to https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/492359

Therefore, I use your source code and give same InputData for test.

Expecting to get 57B4 result, but the incorrect one.

//*****************************************************************************
// includes
//*****************************************************************************
#include "crc_tbl.h"
#include "vcu2_types.h"
#include "vcu2_crc.h"
#include "CrcTable0x1021.h"
#include "CrcTable0x8005.h"
#include "examples_setup.h"

//*****************************************************************************
// defines
//*****************************************************************************
// Filter Symbolic Constants
#define NUM_BYTES       19

//*****************************************************************************
// globals
//*****************************************************************************
#ifdef __cplusplus
#pragma DATA_SECTION("testInput")
#else
#pragma DATA_SECTION(testInput,"testInput")
#endif //__cplusplus

static const uint16_t testInput[NUM_BYTES] = {
		0xA8, 0x01, 0x08, 0x2E, 0xE8,
		0x2E, 0xD0, 0x2E, 0xF0, 0x2E,
		0xE0, 0x2E, 0xE0, 0x2E, 0xE0,
		0x2E, 0xE0, 0x2E, 0xE0
};


// \brief linker generated "run" location for the CRC table object
//
extern uint16_t crcTableRun;
// \brief linker generated "load" location for the CRC table object
//
extern uint16_t crcTableLoad;
// \brief linker generated "size" label indicating the size of the CRC table
// object
//
extern uint16_t crcTableSize;
// \brief object of the structure CRC_Obj
//
CRC_Obj    CRC;
// \brief handle(pointer) to the CRC object
//
CRC_Handle handleCRC;
// \brief A single record(element) from the CRC table object
//

//
uint16_t pass = 0;
uint16_t fail = 0;
extern uint32_t testInputLoadStart, testInputLoadSize, testInputRunStart;

//*****************************************************************************
// protoypes
//*****************************************************************************
// Start of main()
void main()
{
    // Locals
    uint32_t crcResultC_1;
    uint32_t crcResultVcu_1;

#ifdef FLASH
	EALLOW;
	Flash0EccRegs.ECC_ENABLE.bit.ENABLE = 0;
	memcpy((uint32_t *)&RamfuncsRunStart, (uint32_t *)&RamfuncsLoadStart,
			(uint32_t)&RamfuncsLoadSize );
	VCU2_initFlash();
#endif //FLASH
	
	VCU2_initSystemClocks();
	
	VCU2_initEpie();

    //*************************************************************************
    // Example #1: 128 bytes(x8, even), parity: low byte first
    //*************************************************************************
    //! \b Example \b #1, \b Part \b 1
    //! In this section we run a table lookup CRC on the vector testInput. The
    //! table is specified in the header files "CrcTable0x8005.h" and
    //! "CrcTable0x1021.h"respectively and the entries were generated from the
    //! polynomials \f$ x^{16}+x^{15}+x^{2}+1 \f$ (CRC16 802.15.4, 0x8005) and
    //! \f$ x^{16}+x^{12}+x^{5}+1 \f$ (CRC-CCITT, 0x1021) respectively.
    //! The parity chosen was CRC_parity_even indicating that the CRC will start
    //! from the low byte of the first word.
    //! \code
    //************************************************************************
	// This is necessary since the section was declared within a UNION in the linker
	// command file
	memcpy((uint32_t *)&testInputRunStart, (uint32_t *)&testInputLoadStart,
			(uint32_t)&testInputLoadSize );
    // Step 1: Initialize the CRC object
    CRC.seedValue    = INIT_CRC16;
    CRC.nMsgBytes    = NUM_BYTES;
    CRC.parity       = CRC_parity_even;
    CRC.crcResult    = 0;
    CRC.pMsgBuffer   = (uint16_t *)&testInput[0];
    CRC.pCrcTable    = (uint16_t *)&crc16P2Table[0];
    CRC.init         = (void (*)(void *))CRC_init16Bit;
    CRC.run          = (void (*)(void *))CRC_run16BitTableLookupC;

    // Step 2: Initialize the handle
    handleCRC = &CRC;

    // Step 3: Run the 16-bit table look-up CRC routine and save the first result
    CRC.init(handleCRC);
    CRC.run(handleCRC);
    crcResultC_1 = CRC.crcResult;

    //*************************************************************************
    //! \endcode
    //!
    //! \b Example \b #1, \b Part \b 2
    //! Now we run the VCU routine on the vector testInput. The two
    //! polynomials employed by the VCU are  fixed i.e.
    //! \f$ x^{16}+x^{15}+x^{2}+1 \f$ (0x8005) and \f$ x^{16}+x^{12}+x^{5}+1 \f$
    //! (0x1021) respectively
    //! The parity chosen was CRC_parity_even indicating that the CRC will start
    //! from the low byte of the first word.
    //!
    //! Most of the object elements remain unchanged from the initial setup
    //!
    //! \note The VCU routine does not require a lookup table; pCrcTable can be
    //! reset to NULL or left as-is
    //! \code
    //*************************************************************************
    // Step 1: Reset a few elements of the CRC object
    CRC.crcResult    = 0;
    CRC.run          = (void (*)(void *))CRC_run16BitPoly2;

    // Step 2: Run the VCU 16-bit CRC routine and save the result
    CRC.run(handleCRC);
    crcResultVcu_1   = CRC.crcResult;


    // Compare the results of steps 2/3 with 4/5
    (crcResultC_1 == crcResultVcu_1)? pass++ : fail++ ;

    //*************************************************************************
    //!
    //! \endcode
    //!
    //*************************************************************************
    // End of test
    done();
    // Execution never reaches this point
    return 1;
}
// End of main

// @} //addtogroup

// End of file


//###########################################################################
// End of File
//###########################################################################

Thanks!