Part Number: DRV8312-69M-KIT
Hi, everyone,
I bought 2 DRV8312-69M-KITs one month ago, both of them can work well with the GUI of " InstaSPIN_FOC_F2806xM.exe" now, but only one of them can work well with Simulink model of "c28069pmsmfoc_ert.sxl" . The program in the other board always stop automatically after several seconds( I made the status LED blink in my Simuink model, after several seconds, the motor stopped and the LED went out).
ps: the board with num "2016" works well with Simulink model,
the board with num "4312" doesn't work well with Simulink model, the progrom always stop in this board. Matlab:2014a.
I assume these two kits are identical when I bought them, but it seems like there are some difference between these two board.
Does anyone know what the problem is?