Part Number: TMS320F28376D
Hi
i inherited a complex code project in TI CCS and the verify fails to compare with the hex code we have as release.
1) can i dump the flash memory to a file and program it back later? would that work? i have working board and i want the option to program it back in case the code i have does not work?
how to program flash from the dumped file? not from a hex file?
2) is there a utility to change the memory dump to a hex file?
3) is there source code in C/C++ that works with hex files?
thanks,
~loai
tools are CSS 7.0.0 and emulator