This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 341
Part Number: OPA4350
On the F2837x controlCARD devboard, the OPA4350 is used to drive the ADC VREFHI. Actually on my board I used the OPA378 and the OPA625. Could I used the OPA625 to drive the VREFHI of the TMS320F28379D or I must use the OPA4350. What are the critical characteristics to select the rigth opamp for this aplication?
Hi Dany,
The main things to consider here are:
OPA320 => 150uV = 0.2LSBs (12-bit mode, 3.0V reference) = 3.3LSBs (16-bit mode, 3.0V reference)
OPA350 => 500uV = 0.7LSBs (12-bit mode, 3.0V reference) = 10.9 LSBs (16-bit mode, 3.0V reference)
OPA378 => 50uV = 0.1LSBs (12-bit mode, 3.0V reference) = 1.1 LSBs (16-bit mode, 3.0V reference)
OPA625 => 3mV = 4.1LSBs (12-bit mode, 3.0V reference) = 65.5LSBs (16-bit mode, 3.0V reference)
(I just pulled the first max Vos number I saw out of the datasheets, you would also want to add in or ensure this comprehends the operating temperature range of your application)
Note: A chopper-corrected op-amp, while having very low offset error, may not be a good choice for the ADC reference driver because you may see some tones centered at the chopping frequency (and they are usually lower BW).
OPA320 => 20MHz
OPA350 => 38MHz
OPA378 => 900kHz (Note: probably not appropriate for driving the ADC reference)
OPA625 =>120MHz
OPA320 => 7nV / sqrt(Hz) = roughly 0.1 LSBs of peak-to-peak noise (12-bit, 3.0V range, 1MHz BW) or 1.2 LSBs of peak-to-peak noise (16-bit, 3.0V range, 1MHz BW)
OPA350 => 7nv / sqrt(Hz)
OPA378 => 20nv / sqrt(Hz) = roughly 0.2 LSBs of peak-to-peak noise (12-bit, 3.0V range, 1MHz BW) or 3.5 LSBs of peak-to-peak noise (16-bit, 3.0V range, 1MHz BW)
OPA625 => 2.5nV / sqrt(Hz) = roughly 0.0 LSBs of peak-to-peak noise (12-bit, 3.0V range, 1MHz BW) or 0.4 LSBs of peak-to-peak noise (16-bit, 3.0V range, 1MHz BW)
(These are all more than capable for 12-bit operation and the OPA378 is maybe borderline for 16-bit operation, but would probably be OK).
C2000 TI Wiki PagesTI Forum Sitemap
ControlSUITEC2000 Getting Started
CLA FAQsWorkshop Material!
In reply to Devin Cottier: