This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812: How to locate EtherCAT SYNC0 pin on the DSP

Part Number: TMS320F2812


Hi,
I have a seemingly simple question to ask. I want to interface a ET1100 (EtherCAT slave controller) board with my TMS320F2812 DSP. Currently I am using SPI for communication between them. Now I want to include Distributed Clock (DC). From the ET1100 configuration sheet, it is visible that the SYNC/LATCH pin is E11 pin on the board.

Now that is the pin exposed on the ET1100 side. What is the corresponding pin on the TMS320F2812 DSP ???? I ask this because I also have difficulty configuring my SOES (Simple Open EtherCAT Slave) editor. 

(attaching image below) 

  

So summarizing the TWO questions,
1. What is the corresponding SYNC/LATCH pins on the TMS320F2812.
2. What is the configuration setting for this SOES editor? Please note, I don't use AL IRQ.

Any help for these questions is appreciated :) 

Thank you,
Raghu