Part Number: TMS320F28377D
The bootloader of cpu2 in the 28377d is under the control of the CPU1, This figure show the flow after the cpu2 has reset by cpu1. In the stand alone mode the bootmode is controled by Zx-BOOTCTRL register, there are two BOOTCTRL register in the DCSM module ,one is Z1-BOOTCTRL register, another is Z2_BOOTCTRL.
My issue is in the bootloader of cpu2 which register desired the bootmode of cpu2 ?
regards
shook