Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hello,
There is a delay function in my code, where the smallest step is just one microsecond.Could you Please tell me, how will i define my own delay function for smaller steps.
// Included Files
//
#include "F28x_Project.h"
//
// Defines
//
#define BLINKY_LED_GPIO 12
interrupt void xint1_isr(void);
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xS_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xS_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio();
GPIO_SetupPinMux(BLINKY_LED_GPIO, GPIO_MUX_CPU1, 0);
GPIO_SetupPinOptions(BLINKY_LED_GPIO, GPIO_OUTPUT, GPIO_PUSHPULL);
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.XINT1_INT = &xint1_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
//
// Enable XINT1 and XINT2 in the PIE: Group 1 interrupt 4 & 5
// Enable INT1 which is connected to WAKEINT:
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER1.bit.INTx4 = 1; // Enable PIE Group 1 INT4
PieCtrlRegs.PIEIER1.bit.INTx5 = 1; // Enable PIE Group 1 INT5
IER |= M_INT1; // Enable CPU INT1
EINT; // Enable Global Interrupts
// GPIO14 is inputs
//
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 0; // GPIO
GpioCtrlRegs.GPADIR.bit.GPIO14 = 0; // input
GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 0; // XINT1 Synch to SYSCLKOUT only
EDIS;
//
// GPIO14 is XINT1
//
GPIO_SetupXINT1Gpio(14);
//
// Configure XINT1
//
XintRegs.XINT1CR.bit.POLARITY = 1; // Raising edge interrupt 1
//Falling edge interrupt 0
//
// Enable XINT1
//
XintRegs.XINT1CR.bit.ENABLE = 1; // Enable XINT1
//
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Step 6. IDLE loop. Just sit and loop forever (optional):
//
for(;;)
{
}
}
//
// My intrr
//
// xint1_isr - External Interrupt 1 ISR
//
interrupt void xint1_isr(void)
{
//
// Turn on LED
//
GPIO_WritePin(BLINKY_LED_GPIO, 0);
//
// Delay for a bit.
//
DELAY_US(1000*500);
//
// Turn off LED
//
GPIO_WritePin(BLINKY_LED_GPIO, 1);
//
// Delay for a bit.
//
DELAY_US(1000*500);
// Turn on LED
//
GPIO_WritePin(BLINKY_LED_GPIO, 0);
//
// Delay for a bit.
//
DELAY_US(1000*500);
//
// Turn off LED
//
GPIO_WritePin(BLINKY_LED_GPIO, 1);
//
// Delay for a bit.
//
DELAY_US(1000*500);
//
// Acknowledge this interrupt to get more from group 1
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
//
// End of file
//