Tool/software: Code Composer Studio
Dear Mark and Gautam
Thank you very much for your answers to my questions in the thread "What else chips I need to integrate in my own board in order to use the TI F28335 ControlCard?". Now I have further questions based on that.
Can you please also talk about MCU-to-MCU communication? In my project, I need to use four F28335 MCUs (ControlCards) among which there is a MCU (I call it Master MCU) will be in charge of sending/receiving information to/from PC. The other three MCUs will send/receive information to the Master one first and then the PC can see that information through the Master F28335.
For this project, I want to try easy things on the MCU-to-MCU first. That is, if I connect two F28335 MCUs (with the TI USB Docking Station instead of using my own boards that will be developed) to PC, can I just use one CCS to control these two MCUs? If this can be done, then I think I can do the MCU-to-PC communication for the two F28335 MCUs, and then exchange their information within the CCS. If this can be performed, then I can go ahead to think about the MCU-to-MCU communication without the help from the PC.
Can you please help me on the above? Thank you so much for your time.
Lin