Part Number: DRV8301-HC-C2-KIT
Other Parts Discussed in Thread: INSTASPIN-BLDC, DRV8301
I'm unable to start my motor using the DRV8301-HC-C2 kit Rev D and CC2803x ISO DIMM Rev 1.3 control card. I'm using CCS 6.2 and latest control suite install.
The motor is KDE600XF-530-G3 which is 10 Pole.
I'm using 50V power supply supply limited to 6 amps but have a huge capacitor which will supply startup current no problem..
10 Poles and 15k RPM led me to adjust the Vph filter value. I removed the 0.1uF and added a 0.018uF capacitors that put the filter at 1864Hz.
The voltage and current sense circuits should be ok with stock values.
I can't find the software variable in the project you're supposed to change like mentioned in the user guides. Any ideas where USER_VOLTAGE_FILTER_POLE_Hz is?
I went through the labs etc. Loaded the code and adjusted flux threshold to no avail. I tried different control modes. I finally used very long startup ramp times and it will stay on at 100 RPM with advanced startup enabled but you can't adjust duty cycle with the dial.
What am I missing? The pole count can't be selected as 10, i thought that only mattered for RPM feedback?
I've noticed many of the documents don't really match the current state of the projects. Are you supposed to use BLDC_GUI project or just BLDC project that comes with control suite? One has all the motor parameters commented out. The other doesn't.
Thanks!