Tool/software: Code Composer Studio
1. Which is the suitable BAUD rate for 28377s : 9600 or 19200 ?
2. Can wrong BAUD rate be a main reason of wrong appearing of TXDA signals ?
Thanks in advance !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
1. Which is the suitable BAUD rate for 28377s : 9600 or 19200 ?
2. Can wrong BAUD rate be a main reason of wrong appearing of TXDA signals ?
Thanks in advance !
Hi Ed,
eeddii iiiiii said:1. Which is the suitable BAUD rate for 28377s : 9600 or 19200 ?
Generally, these are the baud rates universally preferred: 4800, 9600, 14400, 19200, 38400, 57600, 115200
9600 being the default rate majorly.
eeddii iiiiii said:2. Can wrong BAUD rate be a main reason of wrong appearing of TXDA signals ?
Setting the wrong baud rate can confuse the receiver which would lead to no data display or garbage data display.
Regards,
Gautam
eeddii iiiiii said:If real BAUD rate and set BAUD rate by source code ar not matching , what will be the reason ?
If they're variable, there will be no data transfer. So, you need to match the baud rates!