Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello,
I want to decode differential manchester code at 125kHz. So I need an interuppt every time a transition low/high or high/low occurs and the time difference to the last transition.
For testing purposes I modified the Example_2802xECap_Capture_Pwm.c a little bit, but it just gives me random numbers independent of the input signal. (Tested with my actual signal and a function generator)
I hope you can give me a hint what I have to change in the code.
//########################################################################### // // FILE: Example_2802xECap_Capture_Pwm.c // // TITLE: Capture EPwm3. // // ASSUMPTIONS: // // This program requires the f2802x header files. // // Make the following external connection: // EPWM3 on GPIO4 should be connected to ECAP1 on GPIO5. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2802x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // $Boot_Table // While an emulator is connected to your device, the TRSTn pin = 1, // which sets the device into EMU_BOOT boot mode. In this mode, the // peripheral boot modes are as follows: // // Boot Mode: EMU_KEY EMU_BMODE // (0xD00) (0xD01) // --------------------------------------- // Wait !=0x55AA X // I/O 0x55AA 0x0000 // SCI 0x55AA 0x0001 // Wait 0x55AA 0x0002 // Get_Mode 0x55AA 0x0003 // SPI 0x55AA 0x0004 // I2C 0x55AA 0x0005 // OTP 0x55AA 0x0006 // Wait 0x55AA 0x0007 // Wait 0x55AA 0x0008 // SARAM 0x55AA 0x000A <-- "Boot to SARAM" // Flash 0x55AA 0x000B // Wait 0x55AA Other // // Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger // according to the Boot Mode Table above. Build/Load project, // Reset the device, and Run example // // $End_Boot_Table // // // // DESCRIPTION: // // This example configures EPWM3A for: // - Up count // - Period starts at 2 and goes up to 1000 // - Toggle output on PRD // // eCAP1 is configured to capture the time between rising // and falling edge of the PWM3A output. // //########################################################################### // $TI Release: F2802x Support Library v230 $ // $Release Date: Fri May 8 07:43:05 CDT 2015 $ // $Copyright: Copyright (C) 2008-2015 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Configure the start/end period for the timer #define PWM3_TIMER_MIN 10 #define PWM3_TIMER_MAX 8000 // Prototype statements for functions found within this file. __interrupt void ecap1_isr(void); void InitECapture(void); void InitEPwmTimer(void); void Fail(void); // Global variables used in this example uint32_t ECap1IntCount; uint32_t ECap1PassCount; uint32_t EPwm3TimerDirection; uint32_t DutyOnTime1; uint32_t DutyOffTime1; uint32_t DutyOnTime2; uint32_t DutyOffTime2; uint32_t Period1; uint32_t Period2; // To keep track of which way the timer value is moving #define EPwm_TIMER_UP 1 #define EPwm_TIMER_DOWN 0 void main(void) { // WARNING: Always ensure you call memcpy before running any functions from RAM // InitSysCtrl includes a call to a RAM based function and without a call to // memcpy first, the processor will go "into the weeds" #ifdef _FLASH memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); #endif // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the f2802x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the f2802x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example InitEPwm3Gpio(); InitECap1Gpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the f2802x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in f2802x_DefaultIsr.c. // This function is found in f2802x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.ECAP1_INT = &ecap1_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: InitEPwmTimer(); // For this example, only initialize the EPwm Timers InitECapture(); // Step 5. User specific code, enable interrupts: // Initialize counters: ECap1IntCount = 0; ECap1PassCount = 0; // Enable CPU INT4 which is connected to ECAP1-4 INT: IER |= M_INT4; // Enable eCAP INTn in the PIE: Group 3 interrupt 1-6 PieCtrlRegs.PIEIER4.bit.INTx1 = 1; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Step 6. IDLE loop. Just sit and loop forever (optional): for(;;) { } } void InitEPwmTimer() { EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm3Regs.TBPRD = PWM3_TIMER_MIN; EPwm3Regs.TBPHS.all = 0x00000000; EPwm3Regs.AQCTLA.bit.PRD = AQ_TOGGLE; // Toggle on PRD // TBCLK = SYSCLKOUT EPwm3Regs.TBCTL.bit.HSPCLKDIV = 1; EPwm3Regs.TBCTL.bit.CLKDIV = 0; EPwm3TimerDirection = EPwm_TIMER_UP; EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS; } void InitECapture() { ECap1Regs.ECEINT.all = 0x0000; // Disable all capture interrupts ECap1Regs.ECCLR.all = 0xFFFF; // Clear all CAP interrupt flags ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disable CAP1-CAP4 register loads ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Make sure the counter is stopped // Configure peripheral registers ECap1Regs.ECCTL2.bit.CONT_ONESHT = 0; // Continious Mode ECap1Regs.ECCTL2.bit.STOP_WRAP = 3; // Stop at 4 events ECap1Regs.ECCTL1.bit.CAP1POL = 0; // Rising edge ECap1Regs.ECCTL1.bit.CAP2POL = 1; // Falling edge ECap1Regs.ECCTL1.bit.CAP3POL = 0; // Rising edge ECap1Regs.ECCTL1.bit.CAP4POL = 1; // Falling edge ECap1Regs.ECCTL1.bit.CTRRST1 = 1; // Difference operation ECap1Regs.ECCTL1.bit.CTRRST2 = 1; // Difference operation ECap1Regs.ECCTL1.bit.CTRRST3 = 1; // Difference operation ECap1Regs.ECCTL1.bit.CTRRST4 = 1; // Difference operation ECap1Regs.ECCTL2.bit.SYNCI_EN = 0; // Disable sync in ECap1Regs.ECCTL2.bit.SYNCO_SEL = 3; // Disable ECap1Regs.ECCTL1.bit.PRESCALE = 0; // Prescale = 1 /Disable ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable capture units ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1; // Start Counter ECap1Regs.ECEINT.bit.CEVT4 = 1; // 4 events = interrupt } __interrupt void ecap1_isr(void) { DutyOnTime1 = ECap1Regs.CAP2; // Fetch Time-Stamp captured at T2 DutyOffTime1 = ECap1Regs.CAP3; // Fetch Time-Stamp captured at T3 DutyOnTime2 = ECap1Regs.CAP4; // Fetch Time-Stamp captured at T4 DutyOffTime2 = ECap1Regs.CAP1; // Fetch Time-Stamp captured at T1 Period1 = DutyOnTime1 + DutyOffTime1; Period2 = DutyOnTime2 + DutyOffTime2; __asm(" NOP"); ECap1Regs.ECCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 4 PieCtrlRegs.PIEACK.all = PIEACK_GROUP4; } //=========================================================================== // No more. //===========================================================================