Hi all,
I could able to see the message ids and message data on PCAN with driverlib example code, same code tried with bitfields(there is no message receive handling) is not working as expected, the issue explained in https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/608641
May I Know the reason, any comments are please???
//###########################################################################
//
// FILE: can_external_transmit.c
//
// TITLE: Example to demonstrate CAN external transmission
//
//! \addtogroup cpu01_example_list
//! <h1>CAN-A to CAN-B External Transmit (can_external_transmit)</h1>
//!
//! This example initializes CAN module A and CAN module B for external
//! communication. CAN-A module is setup to transmit incrementing data for "n"
//! number of times to the CAN-B module, where "n" is the value of TXCOUNT.
//! CAN-B module is setup to trigger an interrupt service routine (ISR) when
//! data is received. An error flag will be set if the transmitted data doesn't
//! match the received data.
//!
//! \note Both CAN modules on the device need to be
//! connected to each other via CAN transceivers.
//!
//! \b External \b Connections \n
//! - CANA is on GPIO31 (CANTXA) and GPIO30 (CANRXA)
//! - CANB is on GPIO8 (CANTXB) and GPIO10 (CANRXB)
//!
//! \b Watch \b Variables \n
//! - TXCOUNT - Adjust to set the number of messages to be transmitted
//! - txMsgCount - A counter for the number of messages sent
//! - rxMsgCount - A counter for the number of messages received
//! - txMsgData - An array with the data being sent
//! - rxMsgData - An array with the data that was received
//! - errorFlag - A flag that indicates an error has occurred
//!
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.01.00.00 $
// $Release Date: Mon May 22 15:43:40 CDT 2017 $
// $Copyright:
// Copyright (C) 2013-2017 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h" // Device Headerfile and Examples Include File
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_can.h"
#include "driverlib/can.h"
//
// Defines
//
//#define MSG_DATA_LENGTH 4
#define MSG_DATA_LENGTH 8
#define TX_MSG_OBJ_ID 1
#define RX_MSG_OBJ_ID 1
//
// Globals
//
volatile unsigned long i;
volatile uint32_t txMsgCount = 0;
volatile uint32_t rxMsgCount = 0;
volatile uint32_t errorFlag = 0;
//unsigned char txMsgData[4];
unsigned char txMsgData[8];
unsigned char rxMsgData[4];
tCANMsgObject sTXCANMessage;
tCANMsgObject sRXCANMessage;
//
// Function Prototypes
//
__interrupt void canaISR(void);
//
// Main
//
void main(void)
{
//
// Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
//
InitSysCtrl();
//
// Initialize GPIO and configure GPIO pins for CANTX/CANRX
// on module A and B
//
InitGpio();
//
// Setup GPIO pin mux for CAN-A TX/RX and CAN-B TX/RX
//
GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 5); //GPIO70 - CANRXA
GPIO_SetupPinMux(71, GPIO_MUX_CPU1, 5); //GPIO71 - CANTXA
GPIO_SetupPinOptions(70, GPIO_INPUT, GPIO_ASYNC);
GPIO_SetupPinOptions(71, GPIO_OUTPUT, GPIO_PUSHPULL);
//
// Initialize the CAN controllers
//
CANInit(CANA_BASE);
// Setup CAN to be clocked off the PLL output clock
//
CANClkSourceSelect(CANA_BASE, 0); // 500kHz CAN-Clock
//
// Set up the CAN bus bit rate to 500kHz for each module
// This function sets up the CAN bus timing for a nominal configuration.
// You can achieve more control over the CAN bus timing by using the
// function CANBitTimingSet() instead of this one, if needed.
// Additionally, consult the device data sheet for more information about
// the CAN module clocking.
//
CANBitRateSet(CANA_BASE, 200000000, 500000);
//
// Enable interrupts on the CAN A peripheral.
//
CANIntEnable(CANA_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
//
// Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
// This registers the interrupt handler in PIE vector table.
//
EALLOW;
PieVectTable.CANA0_INT = canaISR;
EDIS;
//
// Enable the CAN-A interrupt on the processor (PIE).
//
PieCtrlRegs.PIEIER9.bit.INTx5 = 1;
IER |= M_INT9;
EINT;
//
// Enable the CAN-A interrupt signal
//
//Enable the CAN-A interrupt signal
CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0);
//
// Initialize the transmit message object used for sending CAN messages.
// Message Object Parameters:
// Message Identifier: 0x5555
// Message ID Mask: 0x0
// Message Object Flags: None
// Message Data Length: 4 Bytes
// Message Transmit data: txMsgData
//
//sTXCANMessage.ui32MsgID = 0x5555;
sTXCANMessage.ui32MsgID = 0x58c;
sTXCANMessage.ui32MsgIDMask = 0;
sTXCANMessage.ui32Flags = 0;
sTXCANMessage.ui32MsgLen = MSG_DATA_LENGTH;
sTXCANMessage.pucMsgData = txMsgData;
//
// Initialize the transmit message object data buffer to be sent
//
txMsgData[0] = 0x01;
txMsgData[1] = 0x23;
txMsgData[2] = 0x45;
txMsgData[3] = 0x67;
txMsgData[0] = 0x89;
txMsgData[1] = 0xab;
txMsgData[2] = 0xcd;
txMsgData[3] = 0xef;
//
// Start CAN module A and B operations
//
CANEnable(CANA_BASE);
//
// Transmit messages from CAN-A to CAN-B //vcm enabled CANA TO CANA
//
while(1)
{
CANMessageSet(CANA_BASE, TX_MSG_OBJ_ID, &sTXCANMessage,
MSG_OBJ_TYPE_TX);
//
// Delay 0.25 second before continuing
//
DELAY_US(1000 * 250);
//
// Increment the value in the transmitted message data.
//
txMsgData[0] += 0x01;
txMsgData[1] += 0x01;
txMsgData[2] += 0x01;
txMsgData[3] += 0x01;
//
// Reset data if exceeds a byte
//
if(txMsgData[0] > 0xFF)
{
txMsgData[0] = 0;
}
if(txMsgData[1] > 0xFF)
{
txMsgData[1] = 0;
}
if(txMsgData[2] > 0xFF)
{
txMsgData[2] = 0;
}
if(txMsgData[3] > 0xFF)
{
txMsgData[3] = 0;
}
}
//
// Stop application
//
asm(" ESTOP0");
}
//
// CAN A ISR - The interrupt service routine called when a CAN interrupt is
// triggered on CAN module A.
//
__interrupt void
canaISR(void)
{
uint32_t status;
//
// Read the CAN-A interrupt status to find the cause of the interrupt
//
status = CANIntStatus(CANA_BASE, CAN_INT_STS_CAUSE);
//
// If the cause is a controller status interrupt, then get the status
//
if(status == CAN_INT_INT0ID_STATUS)
{
//
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Error processing
// is not done in this example for simplicity. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt.
//
status = CANStatusGet(CANA_BASE, CAN_STS_CONTROL);
}
//
// If something unexpected caused the interrupt, this would handle it.
//
else
{
//
// Spurious interrupt handling can go here.
//
}
//
// Clear the global interrupt flag for the CAN interrupt line
//
CANGlobalIntClear(CANA_BASE, CAN_GLB_INT_CANINT0);
//
// Acknowledge this interrupt located in group 9
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP9;
}
//
// End of File
//
*********************************************************************************
Thanks