Hi
A few days ago, I received below answer. I use TMDSHVMTRPFCKIT.
So, I calculate Vd&Vq real voltage _IQmpy(pi_iq.out, _IQ(17.32)).
DC bus voltage is 300V, but instead I used 30V to not change _IQN. 30/sqrt(3) = 17.32.
According to your answers, pi_iq.out 1PU means Vq = 173.2V. Is it right?
I tested following method.
I think that Vs = sqrt(Vd^2 + Vq^2) value is equal to phase peak voltage.
when I run motor 1000RPM, pi_id.out = -0.026 and pi_iq.out = 0.24.
I measured U&V line-to-line rms voltage by multi meter, about 88.8V_rms.
In that case, Vs = 0.242*173.2 = 41.95V.
peak Va = Vab_rms * sqrt(2)/sqrt(3) = 72.5V . not same..
Is there anything wrong with the calculations or theories?
Please give me a detailed explanation! Thanks.