This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: The sdfm module Ierror when start the dma access

Part Number: TMS320F28377D
Other Parts Discussed in Thread: AMC1204

hi,everybody

In my program I set the sdfm modle to sample the current of motor. when i start the dma access to start transfer the data from spidatabuff to emif2. The SDFM module will occurs error Sdfm2Regs.SDIFLG.bit.IFH1. But if i didn't start the DMA transfer this error will not happen. 

As the datasheet description,

In my program the dma access is spirxbuff and the emif interface, the cpu access is sdfm databuff, is there conflict between DMA and CPU? 

if there is the confliction, the conflict will lead to the sdfm module error?

if there is no confliction, why the sdfm module error will happened?

thank you

regards 

shook