Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
①According to Lab1c description, at the very beginning of spin, the motor can not rotate by itself, i have to help the rotor to rotate, after it rotate, i can give the ref_krpm value, the motor speed can be follow the ref value to speed up. how can i make the rotor spin by itself?
the motor parameter is not very complete, it include:
and i have modify the motor parameter in the user.h file, as follows:( I doubt some of these parameter is not very suitable, so the motor can not rotate by itself.)
#elif (USER_MOTOR == Anaheim_BLY172S)
#define USER_MOTOR_TYPE MOTOR_Type_Pm
#define USER_MOTOR_NUM_POLE_PAIRS (3)
#define USER_MOTOR_Rr (NULL)
#define USER_MOTOR_Rs (1.68)
#define USER_MOTOR_Ls_d (0.0006708066)
#define USER_MOTOR_Ls_q (0.0006708066)
#define USER_MOTOR_RATED_FLUX (0.03433958)
#define USER_MOTOR_MAGNETIZING_CURRENT (NULL)
#define USER_MOTOR_RES_EST_CURRENT (1.0)
#define USER_MOTOR_IND_EST_CURRENT (-1.0)
#define USER_MOTOR_MAX_CURRENT (5.0)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (20.0)
#define USER_MOTOR_FREQ_LOW (25.0) // Hz - suggested to set to 10% of rated motor frequency
#define USER_MOTOR_FREQ_HIGH (250.0) // Hz - suggested to set to 100% of rated motor frequency
#define USER_MOTOR_FREQ_MAX (300.0) // Hz - suggested to set to 120% of rated motor frequency
#define USER_MOTOR_VOLT_MIN (3.0) // Volt - suggested to set to 15% of rated motor voltage
#define USER_MOTOR_VOLT_MAX (12.0) // Volt - suggested to set to 100% of rated motor voltage
I have tried much times for these parametes according to the table above, but it still doesn't work. some of parameter i don't know the value is proper, such as USER_MOTOR_FLUX_EST_FREQ_Hz ,
please give me some advice, thanks a lot.