Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hello,
I should work on hysteresis current control for three phase grid connected inverter (2 comparators per each phase), so I need 6 comparators. I found that 28379D microcontroller has 8 WINDOWED comparators.
My question is, could I use internal DACs to program upper and lower boundary for current (hysteresis gap) for all three phases with that 12bit WINDOWED comparators? I should to generate sinusoidal boundaries on frequency of about 10 kHz.
I know that PICCOLO 28027 and 28035 have two 10bit comparators with programmable internal DACs, and they can do that but for only one phase (for one phase application, signal from current sensor is connected on + pin, but on - input of comparator upper of CMP1 and lower boundary of CMP2 from internal DACs are connected)
Thanks in advance!
Nikola.