Tool/software: Code Composer Studio
Hi, I'using a XDS510 USB to debug firmware on a 2837XS and 28334 devices.
By now I virtualized the Xp OS machine where I have the CCS3.3 used for the 334 device and also virtualized the Win10 machine where I have the CCS7 used to develop the 37xS device.
The host computer is a i7 with 24GB RAM and W10 OS.
In this situation when I connect to the external board using the XDS510USB often I loose the communication with the microprocessor and I have to reflash the device to return in trace debug mode.
I think that the XDS510 drive has some problem when run in a virtualized machine.
At this point, also seen that the 64bit driver for the XDS510 will never be done, I'm thinking to buy a Ethernet based device (hope that this bus will be more realible than the USB).
Which is in your exprerience the best cost effective device that I can buy? I'm seeing the XDS220 Ethernet device. Is it a good choiche for a 500Euro target price?
Regards
Giuseppe