Other Parts Discussed in Thread: BOOSTXL-BUCKCONV, SFRA, CODECOMPOSER, LAUNCHXL-F28069M
Tool/software: Code Composer Studio
LAUNCHXL-F28069: BOOSTXL-BUCKCONV
I am working with the LAUNCHXL-F28069 with the Digital Power Buck Converter BoosterPack BOOSTXL-BUCKCONV. I can build the Open Loop Buck Converter Example and run the power supply code on the LAUNCHXL-F28069. However, the LAUNCHXL-F28069 will not show up as a serial COM port on my Windows 10 machine, so I cannot run the SFRA Software Frequency response Analyzer. The error I receive is below.
Debug methods I have tried.
-
Connecting and disconnecting the USB cable to see if the computer will assign the board a COM port.
-
Completely uninstalling CCSv6 and codeComposer studio. And reinstalling.
-
I also found out the XDS100drivers are not digitally signed. So I allowed Windows 10 to install. unsigned drivers and the XDS100driverA and B are installed
The XDS100v2 USB debuggger is working and I can flash and debug the microprocessor.
The XDS100drivers show up as USB controller but do the board does not show up as a Serial COM port.